Unintentional splitting of messages sent via UART using DMA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 3:58 AM - edited ‎2023-09-25 4:00 AM
Hi, I'm having a problem with unintentionally splitting a message I'm trying to send over the UART using DMA . I am using one function to send the message:
const uint32_t max_value_of_counter_loop = 100; /* in case systick jams */
volatile bool was_u1_tx_cplt = true;
HAL_StatusTypeDef OwnTransmitDma(UART_HandleTypeDef *huart, const uint8_t *pData, uint16_t Size)
{
/* Wait on uart to be ready, but no more than 3ms */
uint32_t start_of_try_to_send = HAL_GetTick();
uint32_t counter_while_loop = 0; /* in case systick jams */
while((huart1.gState != HAL_UART_STATE_READY) && (!was_u1_tx_cplt))
{
counter_while_loop++;
uint32_t now_get_tick = HAL_GetTick();
if(now_get_tick > (start_of_try_to_send+2)) break; /* wait no more than 3ms */
if(counter_while_loop > max_value_of_counter_loop) break; /* in case systick jams */
}
was_u1_tx_cplt = false;
return HAL_UART_Transmit_DMA(huart, pData, Size);
}
I call it like this:
uint8_t SendInfoAboutNumberOfStepsMadeByHighPrecisionMotors(uint8_t number_of_axis)
{
int number_of_steps = 0;
uint8_t axis = number_of_axis;
MG_GetNumberOfSteps(axis, &number_of_steps);
Length = sprintf((char*)Message4, "MG%d=%d\n", axis, number_of_steps);
send_status = OwnTransmitDma(&huart1, Message4, Length);
if(send_status != HAL_OK) return RESPONSE_TRY_ERROR;
else return RESPONSE_TRY_OK;
}
I set the was_u1_tx_cplt variable in a callback:
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
if(huart == &huart1) was_u1_tx_cplt = true;
}
Message4 is a global array located in this file:
uint8_t Message4[16];
Not every message is split, moreover 99% of messages are sent without any problems, but sometimes messages are split into two parts and I don't see the dependency when this happens. I don't use RTOS.
I'm using this DMA only for this UART, but also for TX and RX, at first I thought the RX stream was interrupting the TX stream, but I set the TX stream priority to DMA_PRIORITY_MEDIUM where RX has DMA_PRIORITY_LOW and that didn't help.
UART and DMA configuration:
Examples of splitting messages:
Unfortunately, I have no idea what can cause the fact that the significant majority of messages are sent correctly, but some are sent incorrectly. If you have any ideas, please help me with this issue.
STM32F407VGTx,
STM32CubeIDE Version: 1.13.1
Solved! Go to Solution.
- Labels:
-
DMA
-
STM32F4 Series
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:22 AM
But when you wait for HAL_UART_TxCpltCallback , Message4 already has been loaded with the new message.
The DMA will be merrily transmitting the 'old' contents of Message4 and your code overwrites it part way through then waits for DMA to compelte. Sometimes the DMA will be part way through transmitting it, sometimes not.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:08 AM
looks like you calling sprintf( Message4 ...) while Message4 is still being sent out by DMA.
suggest you wait for DMA to complete before loading the next msg into Message4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:14 AM
Waiting for HAL_UART_TxCpltCallback doesn't get the job done? Which interrupt should I wait for?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:18 AM
Try to mark this Message array as volatile.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:21 AM
Anad variable was_u1_tx_cplt too.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:22 AM
But when you wait for HAL_UART_TxCpltCallback , Message4 already has been loaded with the new message.
The DMA will be merrily transmitting the 'old' contents of Message4 and your code overwrites it part way through then waits for DMA to compelte. Sometimes the DMA will be part way through transmitting it, sometimes not.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:26 AM - edited ‎2023-09-25 4:33 AM
ONadr.1
I will try.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:32 AM - edited ‎2023-09-25 4:33 AM
MS.9
Oki, so I understand that I should wait for the HAL_UART_TxCpltCallback not only before sending, but also before the sprintf() function?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 4:38 AM
You should check the was_u1_tx_cplt flag before sprintf and set it to false after sprintf and then start Tx with DMA. When the Tx is complete, the flag is set again in the callback.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-25 5:25 AM
Is it actually splitting it? Or is this how your receiver times out, buffers, or granularity/resolution there.
Check signals on a scope or logic analyzer.
Expect to have to reconstruct data, and resync, on the host. If there are no additional characters inserted, I'd look at other expectations and synchronization
Up vote any posts that you find helpful, it shows what's working..