2020-10-29 7:08 AM
My device NUCLEOF072RB is enumerated as follows = JLINK CDC UART Port (COM5)
I have a STM32 Nucleo board
Now when I am trying to connect to flash the demo program, I am getting the following error
Could not connect to target
Please check power, connection and settings
There is an image also attached below.
Solved! Go to Solution.
2020-10-29 7:22 AM
I figured out the solution. I had to close the ST-Link Pins with the Jumper. I had completely forgot about it
2020-10-29 7:22 AM
I figured out the solution. I had to close the ST-Link Pins with the Jumper. I had completely forgot about it