2022-05-30 8:17 PM
Hi
I'm using Atollic TrueSTUDIO® for STM32, Built on Eclipse Neon.1a. Version: 9.3.0 Build id: 20190212-0734
I get the following error when I try to debug:
STMicroelectronics ST-LINK GDB server. Version 5.1.0
Copyright (c) 2018, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v1.3.0
-------------------------------------------------------------------
Log output file: C:\Users\HLi\AppData\Local\Temp\STM32CubeProgrammer_a17660.log
ST-LINK SN : 55FF6D067880565349412067
ST-LINK FW : V2J31S7
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x415
Device name : STM32L4x1/STM32L475xx/STM32L476xx/STM32L486xx
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: C:\Users\HLi\AppData\Local\Temp\ST-LINK_GDB_server_a17660.srec
File : C:\Users\HLi\AppData\Local\Temp\ST-LINK_GDB_server_a17660.srec
Size : 262184 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 128]
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:00:08.714
Verifying ...
Download verified successfully
Encountered Error when opening C:\Program Files (x86)\Atollic\TrueSTUDIO for STM32 9.3.0\Servers\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...everything was fine before I wrote a few extra functions that pushed from 127 sectors into 128 sectors.
Here is the 127 sector message shows that it was fine before:
STMicroelectronics ST-LINK GDB server. Version 5.1.0
Copyright (c) 2018, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v1.3.0
-------------------------------------------------------------------
Log output file: C:\Users\HLi\AppData\Local\Temp\STM32CubeProgrammer_a16996.log
ST-LINK SN : 55FF6D067880565349412067
ST-LINK FW : V2J31S7
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x415
Device name : STM32L4x1/STM32L475xx/STM32L476xx/STM32L486xx
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: C:\Users\HLi\AppData\Local\Temp\ST-LINK_GDB_server_a16996.srec
File : C:\Users\HLi\AppData\Local\Temp\ST-LINK_GDB_server_a16996.srec
Size : 260424 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 127]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:08.317
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...STM32 ST-LINK Utility loaded the same bin file without error.
The STM32L476 should have 1MB flash, and I've used just over1/4 of it.
I was using no optimization (-O0) when the error occurs. And I have confirmed that with the same code, if I optimize for size (-Os) then the error goes away.
Eventually, my code size will grow and hit this error again.
Please help me get over this limit.
Cheers
Harry
Solved! Go to Solution.
2022-05-31 12:43 AM
Hello @HLi.1047 ,
Try to upgrade firmware version using STM32 ST-LINK Utility: go to ST-LINK>firmware update,
Then disconnect and connect your board.
I also advise you to update the STM32Cubeprogrammer and use the latest release.
Keep us informed about your update.
Imen
2022-05-31 12:43 AM
Hello @HLi.1047 ,
Try to upgrade firmware version using STM32 ST-LINK Utility: go to ST-LINK>firmware update,
Then disconnect and connect your board.
I also advise you to update the STM32Cubeprogrammer and use the latest release.
Keep us informed about your update.
Imen
2022-05-31 4:25 PM
Hi Imen
Thank you so much. Your instructions fixed it.
STM32 ST-LINK Utility showed that I had:
STM32+STM8 Debugger
V2.J37.S7
I reflashed my st-link V2 even though it was the newest firmware.
Then download the newest STM32CubeProgrammer 2.10, installed it, and followed the following instructions to integrate it into TrueStudio:
I had:
STM32CubeProgrammer v1.3.0
Which is very old, I assume it came with TrueStudio, because I never integrated into TrueStudio.
Then everything just worked without optimization.
Cheers
Harry