2008-11-08 10:55 PM
ULINK2 USB-JTAG of Keil and STM3210E-EVAL
2011-05-17 03:51 AM
Dear lev,
Welcome in our STM32 forums :-) Please take care that ''C:\Keil\ARM\Boards\Keil\MCBSTM32E\Blinky'' example and also the other ones under MCBSTM32E sub-directory are done on the following board from Keil and not from ST, so the hardware schematics are not the same. I suggest you to download ST FW library :http://www.st.com/stonline/products/support/micro/files/um0427.zip
, Next go to template project STM32F10xFWLib_v2.0.3\FWLib\project\RVMDK , then replace the files by the ones located in STM32F10xFWLib_v2.0.3\FWLib\examples\GPIO\IOToggle {You can have a look at readme.txt first} to know what is expected to RUN. Hope this helps you. Enjoy it :-) Cheers, STOne-32.2011-05-17 03:51 AM
Shalom from JERUSALEM!
Here is my technical problem: I've got STM3210E-EVAL evaluation board from ST company. - target STM32F103ZE I've tried to programm it's flash with ULINK2 USB-JTAG on the base of simple led blinking test programm. The flash programming is performing, but I cann't see results - the programm not functions. What can I do ? Is it possible use ULINK2 USB-JTAG for STM3210E-EVAL board? Some details: OS : WINDOWS XP IDE-Version: µVision3 V3.63 Copyright (c) Keil Elektronik GmbH / Keil Software, Inc. 1995 - 2008 License Information: LEV USER COMPANY LIC=---- Tool Version Numbers: Toolchain: RealView MDK-ARM Version: 3.24 Toolchain Path: BIN31C Compiler: Armcc.Exe V3.1.0.939 [Evaluation] Assembler: Armasm.Exe V3.1.0.939 [Evaluation] Linker/Locator: ArmLink.Exe V3.1.0.939 [Evaluation] Librarian: ArmAr.Exe V3.1.0.939 [Evaluation] Hex Converter: FromElf.Exe V3.1.0.939 [Evaluation] CPU DLL: SARMCM3.DLL V3.24 Dialog DLL: DARMSTM.DLL V1.36 Target DLL: BIN\UL2CM3.DLL V1.43 Dialog DLL: TARMSTM.DLL V1.35 ************************************************** Listing of main: int main (void) { stm32_Init (); // STM32 setup GPIO_WriteBit(GPIOF, GPIO_Pin_8, Bit_RESET); GPIO_WriteBit(GPIOF, GPIO_Pin_8, Bit_SET); // Turn On Led GPIO_WriteBit(GPIOF, GPIO_Pin_6, Bit_SET); // Turn On Led while (1) { } } ************************************************** Remark: ULINK2 USB-JTAG succesfully works with MCB2300 evaluation board of KEIL Regards Lev Malkin :-[2011-05-17 03:51 AM
Hi,
1.Can you show us body of stm32_Init (); 2. Did you check pin boot0, should be connected to GND.