2018-05-07 5:15 PM
Hi,
I am fairly new to stm32 boards and used the cubeMX program to speed up development for a project I am working on. However, I have found that when sending messages with UART it takes 50ms for each transmit. That seems very slow. Is there a good way to start writing an alternative UART driver for the STMF0RB72T6 or a good open source library I could be directed to? I appreciate any help!
#stm32f02018-05-07 5:33 PM
>>STMF0RB72T6
Going to assume you're super dyslexic.. STM32F072RBT6 ?
http://www.st.com/en/microcontrollers/stm32f072rb.html
What baud rate are you using? How much data are you sending?
The STM32F0 series has SPL, the simpler precursor to HAL/CUBE
http://www.st.com/en/embedded-software/stsw-stm32048.html
The USART registers are also described in the Reference Manual, and programing transfers directly isn't terribly hard.
2018-05-07 9:05 PM
Are your characters being received correctly but slowly? Or are they being garbled as well?
If they are correct, I'd look at the non-cube code that is doing the sending. If they are being garbled, I'd look to see if the various clocks are set up properly.
Different symptoms, different solutions.