Skip to main content
Associate II
Jan 8, 2025 10:11 AM UTC
Solved

UART doesn't work

Hi evryone,

 

I'm trying to initialise a very basic UART communication between my stm32 L552ZE-Q and my computer by following this tutorial: https://www.youtube.com/watch?v=dEQwSl8mCFs&t=924s

 

I have no errors, no warning while compiling and the problem is that there is nothing displayed on the PuTTy teminal. I also used TeraTerm and VScode serial terminal and nothing happened. I tried also on an other computer and same problem.

_Louis__2-1736331047092.png

 

I have upgraded the code by adding a blinking LED to verify if something is even running and the LED is blinking but again nothing on Putty...

 

 while (1)
 {

 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 HAL_UART_Transmit(&huart2, tx_buffer, 27, 10);
	 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_9);
	 HAL_Delay(1000);
 }

 

I've checked the COM port used in my device manager and set the correct Baud rate, I don't know to do next.

_Louis__0-1736330985875.png_Louis__1-1736331018777.png

 

Thank you for your help!

 

Louis

This topic has been closed for replies.
_Louis_Best answer
Associate II
Jan 21, 2025 2:11 AM UTC

Hello,

I found how to enable LPUART1 I just unchecked all the default initialization from cube IDE when creating a project and I can now communicate with my computer with no problems!

Hope that will help somebody!

12 replies

Andrew Neil
Super User
Jan 8, 2025 10:20 AM UTC

@_Louis_ wrote:

_Louis__0-1736330985875.png


So you're using the Virtual COM Port (VCP) in an ST-Link.

What board are you using?

Are you sure that you are using the correct UART - the one that's actually connected to the VCP?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
_Louis_Author
Associate II
Jan 9, 2025 1:36 AM UTC


Hi Andrew,

 

I'm using the NUCLE-L552ZE-Q board.

 


Are you sure that you are using the correct UART - the one that's actually connected to the VCP?


I don't really know, I'm trying to follow the tutorial and adapt it to my board  so I have that on the .ioc file:

_Louis__0-1736386550896.png

The VCP_RX/TX are in reset state so you say that I should try to enable them?

Andrew Neil
Super User
Jan 9, 2025 2:02 AM UTC

@_Louis_ wrote:


I'm using the NUCLE-L552ZE-Q board.


So look at its User Manual to see which UART is connected to the ST-Link's VCP:

AndrewNeil_0-1736388007884.png

https://www.st.com/resource/en/user_manual/um2581-stm32l5-nucleo144-board-mb1361-stmicroelectronics.pdf#page=26

 

As you can see, it's LPUART1 (on PG7, PG8) which is connected to the ST-LINK's VCP

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
Jan 8, 2025 2:56 PM UTC

Not clear how you're initailizing the UART and Pins on the NUCLEO-L552ZE-Q

Doesn't it use LPUART1 on PG7 / PG8? And not USART2

So you'd also have to enable the VDDIO2 for GPIOG

Show code..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
_Louis_Author
Associate II
Jan 9, 2025 1:47 AM UTC

Hi,

I initialized the UART and pins via the .ioc file, Connectivity -> USART2 -> Mode: Asynchronous and  NVIC Settings to activate the USART2 global interrupt as done in the tutorial I follow.

_Louis__0-1736386789308.png

 


@Tesla DeLorean wrote:

Doesn't it use LPUART1 on PG7 / PG8? And not USART2


PA2 an PA3 are configured respectively in USART_TX an USART_RX states and PG7/8 are in reset state.

 


@Tesla DeLorean wrote:

So you'd also have to enable the VDDIO2 for GPIOG


What is it for and how can I do that?

 


@Tesla DeLorean wrote:

Show code..


Do you want any specific part or file or I just dump it there for you?

 

Thank for your time and help!

Andrew Neil
Super User
Jan 9, 2025 2:04 AM UTC

@_Louis_ wrote:

I initialized the UART and pins via the .ioc file, Connectivity -> USART2 


That's the wrong UART!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Karl Yamashita
Principal
Jan 9, 2025 2:57 AM UTC

There seems to be an issue with STM32CubeIDE when trying to enable LPUART1.

As you can see, PG7 and PG8 are in reset state. When selecting LPUART1, the configurations are grayed out so you can't change the Mode.

 

KarlYamashita_0-1736391286118.png

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
_Louis_Author
Associate II
Jan 9, 2025 5:07 AM UTC

@Karl Yamashita wrote:

When selecting LPUART1, the configurations are grayed out so you can't change the Mode.


So there is no way that I can change the mode?

 

Karl Yamashita
Principal
Jan 9, 2025 6:00 AM UTC

You'd have to wait for ST to fix it or you'll have to manually write the configurations. Or try another Nucleo board that doesn't have the same issue.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
_Louis_AuthorBest answer
Associate II
Jan 21, 2025 2:11 AM UTC

Hello,

I found how to enable LPUART1 I just unchecked all the default initialization from cube IDE when creating a project and I can now communicate with my computer with no problems!

Hope that will help somebody!