2020-06-01 11:01 PM
Hello,
I am using STM32CUBEIDE and STM32H743 microcontroller. I want to allocate an array in D2 domain SRAM
I tried the following approach:
1) In the linker script (STM32H743_RAM.ld) i created a separate section called dmabuffer
as follows
.dma_buffer :
{
*(.dma_buffer)
} >RAM_D2
2)In the main.c file declared the array as
uint32_t dmabuffer[1024] __attribute__ ((section(".dma_buffer")));
in main() function
tried loading some value in the dmabuffer
as dmabuffer[0]=0x12345671;
dmabuffer[1]=0x12312311;
3) Uncommented the line /* #define DATA_IN_D2_SRAM */ in the system_stm32hxx.c assuming the D2 domain SRAM is not active by default.
4)But still the array is not being initialised in D2 domain SRAM starting at address( 0x30000000) it is being initialised at D1 Domain SRAM
Looking forward ,
To know any more changes or suggestion on how to declare an array in D2 domain SRAM in STM32H743 microcontroller
Regards,
krishna.
2020-06-02 12:57 AM
Would need to add code in startup.s to copy the initialization data from Flash into RAM, using marker symbols you defined in the linker script.
2020-06-02 1:53 AM
Why do you say it is being initialised at D1 Domain SRAM ?
Do you see the dmabuffer name in the .map file ? What is its address ?
2020-06-02 2:49 AM
Clive is as always correct. Attached is my update to the startup file to load into DTCMRAM. Just change the symbols to match
In startup.s
/* Copy the data segment initializers from flash to DTCMRAM */
movs r1, #0
b LoopCopyDTCMDataInit
CopyDTCMDataInit:
ldr r3, =_siDTCMData
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4
LoopCopyDTCMDataInit:
ldr r0, =_sDTCMData
ldr r3, =_eDTCMData
adds r2, r0, r1
cmp r2, r3
bcc CopyDTCMDataInit
ldr r2, =_sDTCMbss
b LoopFillZeroDTCMbss
/* Zero fill the DTCMbss segment. */
FillZeroDTCMbss:
movs r3, #0
str r3, [r2], #4
LoopFillZeroDTCMbss:
ldr r3, = _eDTCMbss
cmp r2, r3
bcc FillZeroDTCMbss
In loader file
/* used by the startup to initialize data */
_siDTCMData = LOADADDR(.DTCMData);
.DTCMData : {
. = ALIGN(4);
_sDTCMData = .; /* create a global symbol at DTCMData start */
. = ALIGN(4);
*stm32h7xx_it.o (.data .data*)
_eDTCMData = .; /* create a global symbol at DTCMData end */
} >DTCMRAM AT> FLASH
/* Uninitialized DTCM data section */
. = ALIGN(4);
.DTCMbss : {
. = ALIGN(4);
_sDTCMbss = .; /* create a global symbol at DTCMbss start */
. = ALIGN(4);
_eDTCMbss = .; /* create a global symbol at DTCMbss end */
} >DTCMRAM
2020-06-04 9:30 PM
Thanks PMath.4