2021-01-14 7:16 PM
Hi. I'm working on project where I need short pulses with precise periods generated in audio ranges (10 - 20kHz). So I decided to choose TIM2 and using it in PWM mode. I'm using HAL library and configuration code generated by CubeMX:
void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
htim2.Instance = TIM2;
htim2.Init.Prescaler = 2;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 24000;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 150;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_MspPostInit(&htim2);
}
The ARR is changing by TIM4 interrupt which is configured in encoder mode
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Instance == TIM4) {
long value = 24000 + TIM4->CNT * 8;
TIM2->ARR = value;
}
}
So. The freeze occurs when I quickly decreasing TIM4->CNT it takes about 50 seconds after that it starts operating. And it never happened on increasing. For quick test I used this code:
int click = 0;
int main(void) {
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM2_Init();
MX_TIM4_Init();
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
HAL_TIM_Encoder_Start_IT(&htim4, htim4.Channel);
while (1) {
HAL_Delay(2000);
click++;
if (click % 2 == 0) {
TIM2->ARR = 548280;
} else {
TIM2->ARR = 24000;
}
}
}
Could you explain me why is it happens and maybe could point me out to some solution.
Solved! Go to Solution.
2021-01-15 2:22 AM
> htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
If you change ARR below current CNT, CNT keeps incrementing until it overflows over its maximum value to 0, which in case of TIM2 - a 32-bit timer - is cca 4e9 counts (cca 40 seconds if timer's clock is around 100MHz).
The most straighforward solution is to enable ARR preload - this problem is exactly why ARR preload is for.
JW
2021-01-15 2:22 AM
> htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
If you change ARR below current CNT, CNT keeps incrementing until it overflows over its maximum value to 0, which in case of TIM2 - a 32-bit timer - is cca 4e9 counts (cca 40 seconds if timer's clock is around 100MHz).
The most straighforward solution is to enable ARR preload - this problem is exactly why ARR preload is for.
JW
2021-01-15 3:13 AM
Thank you for clear answer!