cancel
Showing results for 
Search instead for 
Did you mean: 

TIM1 break interrupt not firing

bolurian
Associate II

Hi,

I am configuring TIM1 to generate interrupt via MX and I can see that the ISR for TIM1 break is added to the code.
But the interrupt never triggers. I know that break from comparator does happen, but no interrupt!

Does anyone know what could be wrong?

5 REPLIES 5
Billy OWEN
ST Employee

Hi @bolurian 

 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

 

Regards,

Billy

Karl Yamashita
Lead III

Did you set the NVIC?

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
IvanFromCyberia
Associate II

Hello, did you eventually manage to get Break interrupts?

I see the same problem in STM32G431 TIM8.

I can generate all other events interrupts, but cant see neither BREAK nor BREAK2.

I get both breaks flags raised, but no pending interrupts from TIM8.

 

Something is missing.

> I get both breaks flags raised, but no pending interrupts from TIM8.

Read out and check/show content of TIM8 registers.

Generic "interrupt does not fire" checklist here.

JW

IvanFromCyberia
Associate II

What can I say!? RTFM!!!!

Timer has more than 1 interrupt lines.

And!!! Lines are often muxed with it's own or other IPs interrupt lines, when connected to NVIC.

It is different for each timer (T1/T8/T20).

Pay attention to NVIC settings when expect to use certain interrupts!!!

Confusing design, though ... 

Eh ...