cancel
Showing results for 
Search instead for 
Did you mean: 

The value in the WhoAmI register cannot be read properly.

baby_chicken
Associate III

Hi guys,

I am currently trying to read the value of the WhoAmI register using SPI communication with the ICM42688P, but it returns 0xf3 when it should return 0x47.

 

Is there something wrong with my program or configuration?

Please tell me about it.

 

.hpp

 

 

 

 

#pragma once


#include "arm_math.h"
#include "stm32f4xx_hal.h"
#include "stm32f4xx_hal_gpio.h"
#include "spi.h"



class IMUICM42688P {
public:
    IMUICM42688P(SPI_HandleTypeDef &hspi, GPIO_TypeDef *cs_x, uint16_t cs_pin);

    void init();
    uint8_t getWhoAmI();
    float32_t getAccelX();
    float32_t getAccelY();
    float32_t getAccelZ();

private:
    uint8_t read(const uint8_t address);
    void write(const uint8_t address, const uint8_t data);
    void setConfigs();
    void setAccelConfig();
    void setPowerManage();

    SPI_HandleTypeDef &_hspi;
    GPIO_TypeDef *cs_x_;
    const uint16_t cs_pin_;
    float32_t accel_range_;  // default: 2.0f
    float32_t imu_range_;
};

 

 

 

 

 

 

.cpp

 

 

 

 

#include "halplus/layer_driver/circuit/icm42688p.hpp"



IMUICM42688P::IMUICM42688P(SPI_HandleTypeDef &hspi, GPIO_TypeDef *cs_x, uint16_t cs_pin): _hspi(hspi), cs_x_(cs_x), cs_pin_(cs_pin){}


void IMUICM42688P::init(){
    HAL_SPI_Init(&_hspi);
    HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_SET);
    setConfigs();
}

uint8_t IMUICM42688P::getWhoAmI(){
    const uint8_t address = 0x75;   //< Input who_am_i: 0x75, return: 0x47
    return read(address);
}

float32_t IMUICM42688P::getAccelX(){
    const int16_t raw_accel_x = static_cast<int16_t>(((read(0x1F) <<  | read(0x20)));
    return (accel_range_ * static_cast<float32_t>(raw_accel_x) / static_cast<float32_t>(INT16_MAX));
}

float32_t IMUICM42688P::getAccelY(){
    const int16_t raw_accel_y = static_cast<int16_t>((read(0x21) <<  | read(0x22));
    return (accel_range_ * static_cast<float32_t>(raw_accel_y) / static_cast<float32_t>(INT16_MAX));
}

float32_t IMUICM42688P::getAccelZ(){
    const int16_t raw_accel_z = static_cast<int16_t>((read(0x23) <<  | read(0x24));
    return (accel_range_ * static_cast<float32_t>(raw_accel_z) / static_cast<float32_t>(INT16_MAX));
}

uint8_t IMUICM42688P::read(const uint8_t address){
    constexpr uint16_t size = 2;
    const uint8_t read_mode = 0b10000000;  //< (read:1, write:0)
    const uint8_t tx_data[size] = {static_cast<uint8_t>(read_mode | address), 0x00};
    uint8_t rx_data[size] = {0x00, 0x00};

    HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_RESET);  // CS pin: LOW
    HAL_SPI_TransmitReceive(&_hspi, (uint8_t*)tx_data, (uint8_t*)rx_data, size, 100);
    HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_SET);

    return rx_data[1];
}

void IMUICM42688P::write(const uint8_t address, const uint8_t data){
    constexpr uint16_t size = 2;
    const uint8_t tx_data[size] = {address, data};

    HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_RESET);  // CS pin: LOW
    HAL_SPI_Transmit(&_hspi, (uint8_t*)tx_data, size, 100);
    HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_SET);  // CS pin: HIGH
}

void IMUICM42688P::setConfigs(){
    HAL_Delay(10);
    setPowerManage();
    HAL_Delay(10);
    setAccelConfig();
    HAL_Delay(10);
}


void IMUICM42688P::setAccelConfig(){
    constexpr uint8_t accel_conf_addr = 0x50;
    constexpr uint8_t accel_conf_data = 0b01100110;  // range:2[g], rate:1k[Hz]
    write(accel_conf_addr, accel_conf_data);
}


void IMUICM42688P::setPowerManage(){
    constexpr uint8_t accel_conf_addr = 0x4E;
    constexpr uint8_t accel_conf_data = 0b00011111;  // range:2[g], rate:1k[Hz]
    write(accel_conf_addr, accel_conf_data);
}

 

 

 

 

 

 

 

スクリーンショット 2024-08-30 183826.png

Microcontroller STM32F407vgt6,cubeide

Best regards.

 

19 REPLIES 19

Show the wiring diagram. 

Make sure you have a common ground.

Show CLK vs MOSI

Get the clock rate to 1 MHz rather than 10 MHz

 

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

スクリーンショット 2024-09-03 211921.png

スクリーンショット 2024-09-03 211942.png

スクリーンショット 2024-09-03 212001.png

  

Orange is SCLK and blue is MOSI.

Best regards.

This doesn't seem to be correct - there are no pulses on SCK (nor MISO/MOSI).

Double-check the wiring.

JW

TDK
Guru

Not going to catch a 10 MHz signal with a 27 kHz sampling rate.

TDK_0-1725368624701.png

Code seems fine.

If you feel a post has answered your question, please click "Accept as Solution".

スクリーンショット 2024-09-03 224102.png

How much is optimal in this case?

Best regards.

 

Your scaling and what you're capturing is unhelpful. You need to capture the interaction of the data/clocks at the point where you're interacting with the WHOAMI register.

Do you work with someone who has more experience debugging digital circuits and signals?

Perhaps start by drawing a schematic of exactly what you've wired to what.

The make/model of boards the TDK IC is mounted on would also be good contextual information in your presentation of the problem.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

baby_chicken_0-1725373044293.png

Since this module is used for wiring, we assume that the wiring is correct.

Can you tell me what other possibilities there are?

Best regards.

Show waveforms on the bus taken by oscilloscope, this time set with proper sampling rate (i.e. at least 4x the SPI baudrate, but more is preferrable).

JW

Looks to be stock imagery, some chance you can share YOUR wiring implementation?

https://strawberry-linux.com/catalog/items?code=42688

>>Can you tell me what other possibilities there are?

There are a lot of opportunities to fail, far fewer to do things correctly and succeed.

VDD + VDDIO to 3.3V

GND to GND

-CS to GPIO

SCLK to SPIx_SCLK

SDO to SPIx_MISO

SDI to SPIx_MOSI

 

I'd probably avoid HAL_SPI_Transmit() and use HAL_SPI_TransmitReceive() into a scratch buffer, the former is apt to complete early and the CS go high prior to completion.

The signals you want to look at are where it's physically interacting with the part, you'll see the data bits going out, the clocks, and the data bits coming back.

Large traces with nothing happening on them isn't helpful. Are the GPIO pins correctly configured? Can you capture the actual interaction and response? Can you find a Logic Analyzer?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for your response.

 

Changed program to use HAL_SPI_TransmitReceive().

#include "halplus/layer_driver/circuit/icm42688p.hpp"

#define WHO_AM_I 0x75
#define PWR_MGMT_0 0x4E
#define DEVICE_CONFIG 0x11
#define DRIVE_CONFIG 0x13
#define GYRO_CONFIG 0x4F

ICM42688P::ICM42688P(SPI_HandleTypeDef &hspi, GPIO_TypeDef *cs_x, uint16_t cs_pin): hspi_(hspi), cs_x_(cs_x), cs_pin_(cs_pin){}

uint8_t ICM42688P::read_byte(uint8_t reg) {

	  uint8_t rx_data[2];
	  uint8_t tx_data[2];

	  tx_data[0] = reg | 0x80;
	  tx_data[1] = 0x00;  // dummy

	  HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_RESET);
	  HAL_SPI_TransmitReceive(&hspi_, tx_data, rx_data, 2, 1);
	  HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_SET);

	  return rx_data[1];
}//rx:receive,tx:transmit

void ICM42688P::write_byte( uint8_t reg, uint8_t val) {

	  uint8_t rx_data[2];
	  uint8_t tx_data[2];

	  tx_data[0] = reg & 0x7F;
	  tx_data[1] = val;  // write data

	  HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_RESET);
	  HAL_SPI_TransmitReceive(&hspi_, tx_data, rx_data, 2, 1);
	  HAL_GPIO_WritePin(cs_x_, cs_pin_, GPIO_PIN_SET);
}
void ICM42688P::setup() {

	  uint8_t who_am_i;

      HAL_Delay(50); // wait start up
	  who_am_i = read_byte(WHO_AM_I); // 1. read who am i
	  printf( "who : 0x%x\n",who_am_i); // 2. check who am i value

	  // error check
	  if ( who_am_i != 0x47){
	    while(1){
	      printf( "gyro_error\r");
	    }
	  }

	  HAL_Delay(50); // wait

	  write_byte(DEVICE_CONFIG, 0x00);

	  HAL_Delay(50);

	  write_byte(PWR_MGMT_0, 0x1F); // set pwr_might

	  HAL_Delay(50);

	  write_byte(DRIVE_CONFIG, 0x03); // set config

	  HAL_Delay(50);

	  write_byte(GYRO_CONFIG, 0x06); // set gyro config 32kHz 2000dps

	  HAL_Delay(50);
}

.hpp

#pragma once

#include <stdio.h>
#include <stdint.h>
#include "spi.h"
#include "stm32f4xx.h"
#include "stm32f4xx_hal_spi.h"
//#include "arm_math.h"

class ICM42688P {
public:
    ICM42688P(SPI_HandleTypeDef &hspi, GPIO_TypeDef *cs_x, uint16_t cs_pin);

    uint8_t read_byte(uint8_t reg);
    void write_byte(uint8_t reg, uint8_t val);
    void setup();

private:
    SPI_HandleTypeDef &hspi_;
    GPIO_TypeDef *cs_x_;
    uint16_t cs_pin_;
};

The change to this program returned the value of the WhoAmI() register as 0x0.

 

Wiring is done referring to this image.

baby_chicken_0-1725411012839.png

 

Sorry, I have been disconnecting the module and looking at the signal.
Should I just put the module back on and check the SDI and SDO signals?
Sorry for repeating myself, but thank you in advance.