cancel
Showing results for 
Search instead for 
Did you mean: 

the max frequency of STM32G030x6x8 series CORE

stephenliu
Associate

hi,everyone,I'm a new user of the SMT32 MCU, now i'm looking up the datasheet of STM32G030x6/x8 series, In this article, the Frequency of CORE is described to reach up 64MHz on PAGE 1, but on PAGE 11, Figure 11 block diagram, fmax = 56MHz, so what I want to asked is which one is correct ?

2 REPLIES 2
gbm
Lead III

64 MHz is the specified maximum for production chips. 56 MHz looks like a leftover from pre-production document.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
stephenliu
Associate

Thanks for your kindly reply, and I have another question, now I got a STM32 Nucleo-64 board,but i can't find the demo source code in ST website,would you please tell me where I can download the demo program? What i mean is not the STM32Cube_FW_G0_V1.5.0 package, but the real program run on this board while power up