2019-11-28 07:40 AM
the debugger of IAR EARM V8 has lots of bugs in tracking C codes sentences, has anybody experienced it and find a solution?
V7 is pretty stable but no support for many recent ST MCUs, I think F7(not all of them), H7, L4+
any idea to add these MCU as packages to V7?
2019-11-28 07:57 AM
There were IAR (7) patches in the PC_Software nodes of some of the CubeH7, etc packages.
If you're a paying IAR customer you should take up support issues with them directly. If you're still unsatisfied vote with your feet, demand a refund and walk away.
ST FAE's may also have patches.
2019-11-28 08:00 AM
Mirrored H7 IAR files latter half of this thread
https://community.st.com/s/question/0D50X00009kIxoZSAS/iar-configurations-for-stm32h7
2019-11-28 09:44 AM
Are these patches to integrate unsupported MCUs to v7?