cancel
Showing results for 
Search instead for 
Did you mean: 

Target not found error in STM32H743ZI2

suhfi
Senior

i am using nucleo-144, H743ZI2 board. while i am uploading code in the stm32cubeide i am getting error as "target not found". i have searched in the community and then tried connect the boot0 to high, and power the board, connect to cube programmer and erase full chip flash memory. while i do that i am not able to connect board. i am getting an error as: no stm32 target found. i have tried to connect boot 0 to vcc and power it. In the cube programmer i am unable to get the connect. and i have gone through the user manual of the board h743zi2 board, but there also i received the same answer. when i connect or power the board, we get the firmware right, i am getting mbed, details and failed also. in the fail text document i have "The interface firmware FAILED to reset/halt the target MCU". what should i do? I want to upload the new code and will it be possible to erase the old code.

27 REPLIES 27

yeah, from vdd and jp4 i got 5volts power. and i did power my board from the USB PWR(CN1) to the usb of the laptop.

5V as VDD would for sure break your MCU.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

yeah, when vdd_mcu i got 5volts power from multimeter. and for the power i am giving usb_pwr(CN1) to the usb of the laptop

A host pc connected to CN1 through USB cable is how i powered my board.

SofLit_0-1725534787284.png

Are you sure you measured the voltage level on these points? and you connect the cable to CN1 USB cable?

Because it doesn't make sense to get 5V on VDD_MCU on JP4.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
suhfi
Senior

yes, i have got that on vdd. and the power i am using is usb pwr(CN1) to the usb cable connected to the laptop

Unfortunately, I think your board is broken (may be the 3.3V regulator was burned inducing to pass the previous regulator 5V voltage?) as well as your MCU.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

so, the thing is i measured it wrong. now when i correct it i am getting it as 0volts nearly. so i guess my board isn't broken. what is this 0 volts. how much should i get and everything?


@suhfi wrote:

so, the thing is i measured it wrong. now when i correct it i am getting it as 0volts nearly. so i guess my board isn't broken. what is this 0 volts. how much should i get and everything?


Sorry, I didn't understand. Please be more concise in order to avoid unnecessary ping pong and converge to a solution.

You need to post a picture of your board with an ST-LINK connection and show how do you measure VDD_MCU using a multimeter or something else ..

Thank you for your understanding.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

So, sorry for miscommunication from my behalf. I wanted to say that i have checked voltage in a wrong way. and after seeing the picture you shared me, i did it the right way and i am getting 0volts. and so i have a question. how much exactly i should get ?