‎2021-03-19 02:34 AM
Hi everyone, I am currently working on a project working on a STM32F469I-DISCO. I would like to be able to use the embedded RTC as well as the backup SRAM. I have seen on the schematic that the VBAT pin is tied up to the 3.3V. Is there a way to still supply voltage to the VBAT pin (through the 3.3V for exemple) ?
Thank you.
Solved! Go to Solution.
‎2021-03-19 04:17 AM
Looking at gerbers of rev.C, it appears that the VBAT track is on bottom, appears to be quite well accessible.
If this is a one-off and you have some skills with cutting/joining PCB tracks (i.e. the usual techniques used to fix botched prototypes which are otherwise OK), it could be cut and brought out to some suitable point.
JW
‎2021-03-19 03:48 AM
Unfortunately, no.
The more dense DISCO boards are unfortunately not very well designed with respect to general usability. ST's strategy moved from DISCO boards as a vehicle for having joy through experimentation, towards Nuclei as barebone board, and Discos being shiny but single-purpose boards.
As I've said too many times, ST does not understand the reason of the STM32's success.
JW
‎2021-03-19 03:50 AM
That's too bad ... My company wanted to avoid designing our own board but it may be something to think about then ...
‎2021-03-19 04:17 AM
Looking at gerbers of rev.C, it appears that the VBAT track is on bottom, appears to be quite well accessible.
If this is a one-off and you have some skills with cutting/joining PCB tracks (i.e. the usual techniques used to fix botched prototypes which are otherwise OK), it could be cut and brought out to some suitable point.
JW
‎2021-03-19 04:49 AM
Thank you a lot for your input. Unfortunately, this would not be a one off as we plan to use this board for a project which will be commercialized
‎2021-03-19 04:56 AM
The use in a commercial product is not permitted anyway, see the Evaluation Board Terms Of Use:
The Evaluation Board shall not be, in any case, directly or indirectly assembled as a part in any production of Yours as it is solely developed to serve evaluation and testing purposes and has no direct function and is not a finished product.
Regards
/Peter
‎2021-03-19 04:58 AM
Ow, I wasn't aware of that ... Guess we will have to design our own board and then the VBAT will be accessible!
‎2021-03-19 05:13 AM
No problem. It seldom happens that the Terms of Use are read. 😀
Good luck!
When your question is answered, please close this topic by choosing Select as Best for the favourite answer. This will help other users find that answer faster.
/Peter