cancel
Showing results for 
Search instead for 
Did you mean: 

STPM32 Regulator outputs

Mehmet Alper  USLU
Associate
Posted on November 03, 2017 at 20:49

Hi,

It is shown at the schematic of EVALSTPM32 evaluation board , both 3V and 1.2V voltage regulator outputs are connected to ground via some capacitors. Is it mandatory to terminate these pins as shown in the schematic of EVALSTPM32 even if we don't use regulator outputs? I mean can we left these pins open?

Note: I attached the schematic of EVALSTPM32.

Kind Regards,

Alper

#stpm32 #stpm33
0 REPLIES 0