ADC_DMAHalfConvCplt called when the buffer is completely full
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-02 8:13 AM
Hello,
I am running the ADC_DMA_Transfer example on NUCLEO-H743ZI without any changes. And i see the ADC_DMAHalfConvCplt getting called when the aADCxConvertedData buffer is completely full and not half full as expected.
Am i missing something? Shouldn't
ADC_DMAHalfConvCplt be called after ADC_CONVERTED_DATA_BUFFER_SIZE/2 conversions instead of after ADC_CONVERTED_DATA_BUFFER_SIZE?
I do see ADC_DMAConvCplt being called every time after ADC_DMAHalfConvCplt, but it seems like after a call to either of these functions all the content in buffer is replaced.
Thanks,
Evgeny
#dma-adc #dma #adc #stm32h743- Labels:
-
ADC
-
DMA
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-03 11:19 AM
I did a couple of experiments, looks like i was 'fooled' by the IDE. If , during half conversion complete event, i copy the whole buffer to a different location, i can see that indeed a bit more than half buffer was filled. Same goes for conversion complete event. So it looks like there is a big delay from the point that DMA raises the interrupt until the IDE shows me the buffer, the DMA is able to fill the remaining half......