cancel
Showing results for 
Search instead for 
Did you mean: 

STMG0 Multichannel ADC CubeIDE configuration issue

Gaston
Associate III

Hi,

I'm not able to set the STM32G030C6 ADC1 for 9 + Internal Temperature Sensor channels. Here's my ADC1 Mode and Configuration parameters

 

Gaston_1-1719938564685.png

Gaston_2-1719938744194.png

I'm using this recently updated Software Package Version

STM32CubeG0 Firmware Package V1.6.2

Does anyone know what the problem is?

Regards,
Gaston

3 REPLIES 3
KnarfB
Principal III

no such errors here with STM32CubeMX 6.11.1. Conflicts with other peripherals?

Screenshot 2024-07-02 195740.png

No. It does not work with latest CubeIDE v1.16 (CubeMX v6.12) update.

I've downgraded the iDE to v1.15.2 (CubeMX 6.11.1) and it works fine.

It seems a CubeIDE v1.16 issue

EdwinID
Associate II

Hi. Same problem here. It seems to have something to do with setting the sequencer to not fully configurable.

I've started a new clean project, STM32G070RBTx, only configure one pin on the ADC tab, set sequencer to not fully configurable, and the error appears

EdwinID_0-1720185024725.png

Regards,

Edwin