STM32U5A5 -- I2C Timeout waiting for TXIS flag --
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-07 8:53 AM
Hello all,
I have been trying to get I2C communication working on my NUCLEO-U5A5ZJ-Q board based on STM32U5A5ZJJT6U. First I have used STM32-CUBE-IDE and CUBE-MX to generate code but I was getting error when I try to transmit so I write a custom code which is also attached attached and after doing a bit of stepping through the code, it looks as though a HAL_TIMEOUT occurs when the I2C driver executes the I2C_WaitOnTXISFlagUntilTimeout() function and the exact error I am getting is as below
if ((__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_TXIS) == RESET))
{
hi2c->ErrorCode |= HAL_I2C_ERROR_TIMEOUT;
hi2c->State = HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_ERROR; /// HERE IT RETURNS ERROR IN MY CASE ///////
}
I have looked through the datasheet for this particular micro to figure out why this flag would not be set, but it is not immediately clear and it is controlled by HW. Is there something wrong with my setup?
Also I have changed main as follow:
int main(void)
{
HAL_Init(); // Initialize the HAL library
SystemClock_Config(); // Configure the system clock
__HAL_RCC_GPIOB_CLK_ENABLE(); // Enable GPIOB clock
__HAL_RCC_I2C1_CLK_ENABLE(); // Enable I2C1 clock
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1; // Configure GPIO pins for I2C1 SCL and SDA
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD; // Alternate function open-drain
GPIO_InitStruct.Pull = GPIO_PULLUP; // Enable internal pull-up resistors
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; // High-speed output
GPIO_InitStruct.Alternate = GPIO_AF4_I2C2; // I2C1 alternate function
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct); // Initialize GPIO pins
hi2c1.Instance = I2C2; // Select I2C1 peripheral
//hi2c1.Init.Timing = 0xE14;
hi2c1.Init.Timing = 0x30420F13;
//hi2c1.Init.ClockSpeed = 100000; // I2C clock speed (100 kHz)
//hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; // I2C duty cycle
hi2c1.Init.OwnAddress1 = 0; // Not used in master mode
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; // 7-bit addressing mode
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; // No dual addressing
hi2c1.Init.OwnAddress2 = 0; // Not used in master mode
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; // No general call
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; // Enable clock stretching
if (HAL_I2C_Init(&hi2c1) != HAL_OK) // Initialize I2C peripheral
{
Error_Handler(); // Handle initialization error
}
uint8_t sendData[] = {0x01}; // Data to be sent over I2C
while (1)
{
if (HAL_I2C_Master_Transmit(&hi2c1, 0x20, sendData, sizeof(sendData), 10000) != HAL_OK)
{
Error_Handler(); // Handle transmission error ////////////////////// HERE ITS RETURNING ERROR AFTER TIME OUT EXPIRE ///////////////////////////
}
}
}
Any help would be greatly appreciated.
Thanks!
- Labels:
-
Bug-report
-
I2C
-
STM32CubeMX
-
STM32U5 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-07 12:37 PM - edited ‎2024-02-07 12:37 PM
> hi2c1.Instance = I2C2
Clearly this is a modification you've done (among others). Unless you have deep insight into how CubeMX is generating code and how HAL uses that code, I wouldn't make such modifications.
I would go back and use CubeMX generated code as-is rather than modifying it.
If you want to use I2C2 instead of I2C1, change it in CubeMX and regenerate the code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-07 9:13 PM
Hello ahsank,
After looking at your code it seems like you are using I2C2 for the communication purpose. You are using PF0 and PF1 for SDA and SCL. But while initializing clock you have enabled GPIO Port B clock(Change it to GPIOF's Clock).Also initialize I2C2 peripherial instead of I2C1 as mentioned by @TDK ,.
Hope after rectification it may work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-08 7:19 AM
I have recreated new project using cube IMX and use I2C2 PF0 and PF1 but not getting any output , I have been using picoscope to see it
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-08 7:28 AM
if i just toggle PF0 and PF1 I am getting correct output but If I send data using i2c using following main while loop and obv configuration done by cube IMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-08 9:11 PM
Dear @ahsank ,
Can you please share your latest configuration for I2C2 peripheral. Also tell what I2C peripheral you are using(Is it Arduino board, LCD, or something else.)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-09 6:20 AM
static void MX_I2C2_Init(void)
{
/* USER CODE BEGIN I2C2_Init 0 */
/* USER CODE END I2C2_Init 0 */
/* USER CODE BEGIN I2C2_Init 1 */
/* USER CODE END I2C2_Init 1 */
hi2c2.Instance = I2C2;
hi2c2.Init.Timing = 0x00000E14;
hi2c2.Init.OwnAddress1 = 0;
hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c2.Init.OwnAddress2 = 0;
hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c2) != HAL_OK)
{
Error_Handler();
}
Here is configuration of i2S I am using , it is created by Mx-Cube
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C2_Init 2 */
/* USER CODE END I2C2_Init 2 */
}
I am not using any i2c peripheral at a moment.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-09 7:03 AM
What board is this?
Do you have pullups on SDA/SCL lines? If so what values?
What waveform do you see on SDA/SCL during a HAL_I2C_IsDeviceReady call?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-09 8:45 AM - edited ‎2024-02-09 8:47 AM
its a NUCLEO-U5A5ZJ-Q board
I have tried by enabling and disabling pullups but no success
The configuration when pullup enabled is as follow
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOF, GPIO_PIN_0|GPIO_PIN_1, GPIO_PIN_RESET);
/*Configure GPIO pins : PF0 PF1 */
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
the wave for SDA and SCL is shown as below
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-02-09 11:18 AM
Not sure I understand this test. You've initialized PF0 and PF1 as GPIO outputs and set them to a low level. They look to be low on your scope. That all is functioning as expected, yes?
If you want PF0/PF1 to be I2C pins, you need to initialize them as such. CubeMX should generate the code to do this for you.