2024-04-13 10:51 AM
I'm trying to work with USB on STM32U595ZJT6Q (with SMPS)
Ref Clock Selection under USB_OTG_HS is set to 16MHz
OTS HS Clock Mux is set to HSE (the board has 16MHz crystal)
CubeMX 6.11
STM32Cube_FW_U5_V1.5.0
The code is stuck in USB_CoreReset, more specifically it waits for USB_OTG_GRSTCTL_CSRST to become 0
do
{
count++;
if (count > HAL_USB_TIMEOUT)
{
return HAL_TIMEOUT;
}
} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);
After searching the forum I discovered that CubeMX is not generating __HAL_RCC_SYSCFG_CLK_ENABLE call in HAL_PCD_MspInit. However, after adding this call nothing changes.
void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(pcdHandle->Instance==USB_OTG_HS)
{
/* USER CODE BEGIN USB_OTG_HS_MspInit 0 */
__HAL_RCC_SYSCFG_CLK_ENABLE();
/* USER CODE END USB_OTG_HS_MspInit 0 */
Can someone help me resolve the issue?
Solved! Go to Solution.
2024-04-13 1:55 PM
Okay, I think I figured it out. SYSCLK has to be more than 48MHz. Just changing it to 64 MHz fixed an issue.
2024-04-13 11:00 AM
Do you set the USB clock to 48Mhz ?
I don't understand what you wrote.
2024-04-13 11:04 AM
It's not even possible to set 48MHz with U5 series
2024-04-13 11:36 AM
Ok, sorry - 48M is mandatory for full speed , but you set it to hi speed . So ok , but i wouldn't choose the lowest clk.
btw
I found in similar H5 USB setting : the power enable was missing - so check, if this is there.
I added in xxx_hal_msp.c :
in
void HAL_HCD_MspInit(HCD_HandleTypeDef* hhcd)
/* USER CODE BEGIN USB_DRD_FS_MspInit 1 */
HAL_PWREx_EnableVddUSB();
/* USER CODE END USB_DRD_FS_MspInit 1 */
2024-04-13 11:51 AM
void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(pcdHandle->Instance==USB_OTG_HS)
{
/* USER CODE BEGIN USB_OTG_HS_MspInit 0 */
__HAL_RCC_SYSCFG_CLK_ENABLE();
/* USER CODE END USB_OTG_HS_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USBPHY;
PeriphClkInit.UsbPhyClockSelection = RCC_USBPHYCLKSOURCE_PLL1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/** Set the OTG PHY reference clock selection
*/
HAL_SYSCFG_SetOTGPHYReferenceClockSelection(SYSCFG_OTG_HS_PHY_CLK_SELECT_6);
/* USB_OTG_HS clock enable */
__HAL_RCC_USB_OTG_HS_CLK_ENABLE();
__HAL_RCC_USBPHYC_CLK_ENABLE();
/* Enable VDDUSB */
if(__HAL_RCC_PWR_IS_CLK_DISABLED())
{
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddUSB();
/*configure VOSR register of USB*/
HAL_PWREx_EnableUSBHSTranceiverSupply();
__HAL_RCC_PWR_CLK_DISABLE();
}
else
{
HAL_PWREx_EnableVddUSB();
/*configure VOSR register of USB*/
HAL_PWREx_EnableUSBHSTranceiverSupply();
}
/*Configuring the SYSCFG registers OTG_HS PHY*/
/*OTG_HS PHY enable*/
HAL_SYSCFG_EnableOTGPHY(SYSCFG_OTG_HS_PHY_ENABLE);
/* USB_OTG_HS interrupt Init */
HAL_NVIC_SetPriority(OTG_HS_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(OTG_HS_IRQn);
/* USER CODE BEGIN USB_OTG_HS_MspInit 1 */
/* USER CODE END USB_OTG_HS_MspInit 1 */
}
}
There is an HAL_PWREx_EnableVddUSB() call that is executed (line 40).
Also tried 24MHz and 32MHz by using the PLL(16MHz was from HSE). Maybe it's a good option to physically change the crystal for a 24/32MHz one?
2024-04-13 12:02 PM
Ok, so PWREx_Enable seems not the problem here.
+
> to physically change the crystal for a 24/32MHz one?
No, this is just the reference clock, you set in clock tree , what you want; it should be no difference, what crystal is used. I always prefer a standard frequency here, 8 or 16 M .
Just - what i dont understand : is line 36 :
__HAL_RCC_PWR_CLK_DISABLE();
I would comment out this - just to test, what happens...and/replace with xxx_ENABLE () .
2024-04-13 12:10 PM
if(__HAL_RCC_PWR_IS_CLK_DISABLED())
{
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddUSB();
/*configure VOSR register of USB*/
HAL_PWREx_EnableUSBHSTranceiverSupply();
__HAL_RCC_PWR_CLK_DISABLE();
}
else
{
HAL_PWREx_EnableVddUSB();
/*configure VOSR register of USB*/
HAL_PWREx_EnableUSBHSTranceiverSupply();
}
Because __HAL_RCC_PWR_IS_CLK_DISABLED check is failed only else branch is being executed.
However just to be safe I tried commenting and changing to ENABLE, still to luck.
2024-04-13 1:55 PM
Okay, I think I figured it out. SYSCLK has to be more than 48MHz. Just changing it to 64 MHz fixed an issue.