cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F722 timeout in USB_CoreReset()

Raees
Associate III

It's working now. But I have to comment this line __HAL_RCC_USB_OTG_HS_ULPI_CLK_ENABLE(); line in the CubeIDE generated code for it to work

1 REPLY 1
KDJEM.1
ST Employee

Hello @Raees ,

Moved from: Solved: Re: STM32U595 timeout in USB_CoreReset() - STMicroelectronics Community

Thank you for bringing this issue to our attention.

I reported this issue internally.

Internal ticket number: 186324 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.