Skip to main content
DReis.2
Associate II
October 14, 2021
Solved

STM32L4S9 OctoSPI PSRAM support

  • October 14, 2021
  • 3 replies
  • 2695 views

Hi,

I work with a development team that is developing a product that has a STM32L4S9 MCU and a IS66WVH8M8ALL-100 HyperBus PSRAM.

Recently, we found in the STM32L4 Errata that actually this MCU does not support PSRAM. We noticed that the self-refresh was not occuring and data was being lost/corrupted.

We tried changing the OctoSPI configuration, but any attempt did not work.

0693W00000FCV2bQAH.png 0693W00000FCV48QAH.png0693W00000FCV5QQAX.png 

We measured nCS pin, and in fact it is not released in time (4us) to allow the refresh to occur.

0693W00000FCV6sQAH.pngIn our project we use this memory configured as memory mapped, so we can extend the internal memory . The RAM is used to save various user data, framebuffers and more.

By looking at the HAL code we see that there is a memory type HAL_OSPI_MEMTYPE_MACRONIX_RAM. But we could not find any other OctoSPI RAM memory that is not PSRAM and has density of 64Mb (8MB).

I wonder if someone has faced this same problem and could use, maybe, some OctoSPI Static RAM instead, that does not require self-refresh function.

*We already know and tested a STM32H7 MCU using the same PSRAM, and it fully works. However, this will require a huge change in our product, so we are trying to first understand all options around the STM32L4S9 MCU

This topic has been closed for replies.
Best answer by Alex - APMemory

Hi,

I confirm ST doesn't support OPI configuration on this specific version of MCU. following version are supporting IoT RAM (QSPI or OPI PSRAM). One alternative option could be to use ADMUX PSRAM on FMC bus.

fyi, we still have few customers who manage to run our memory for frame buffering (64Mb IoT RAM APS6408L-OBM for example). Key point is you need to avoid odd address write issue. In their use case, since the pixel was 2 bytes, the DMA2D should be 2 bytes aligned, so they had no odd address access.

Regards

Alex

3 replies

Alex - APMemory
Alex - APMemoryBest answer
Associate II
November 29, 2021

Hi,

I confirm ST doesn't support OPI configuration on this specific version of MCU. following version are supporting IoT RAM (QSPI or OPI PSRAM). One alternative option could be to use ADMUX PSRAM on FMC bus.

fyi, we still have few customers who manage to run our memory for frame buffering (64Mb IoT RAM APS6408L-OBM for example). Key point is you need to avoid odd address write issue. In their use case, since the pixel was 2 bytes, the DMA2D should be 2 bytes aligned, so they had no odd address access.

Regards

Alex

DReis.2
DReis.2Author
Associate II
November 29, 2021

Thanks for your reply @Alex - APMemory​ 

We do run our IS66WVH8M8ALL with framebuffer the same way (16 bit color), and it works. However we had problems using more general data, so we decided changing to STM32H7 MCU to fully support the OSPI PSRAM.

Best Regards

Alex - APMemory
Associate II
November 29, 2021

OK, good to hear

If you need a compatible alternative in current tight period you can check APS6408L-OBM-BA.

Alex