2018-01-14 1:34 AM
Hi everyone,
Should I connect a any series resistor to the super capacitor while using a super capacitor that is 1F 5.5V instead of a battery? Or I can connect directly the capacitor to VBat pin?
#power-backup-supercapacitor-rtc #rtc2018-01-14 12:37 PM
Turvey.Clive.002
is right to say we avoid batteries. with the extra handling issues since they are live 24/7Sahin.Gokhan
is right to ask if a cap would do, great solutionBonnes.Uwe
is quite right to suggest the CR2032 style lithium. also good solutionAircraft / delivery are always an issue with batteries. this is a big issue
The best solution is to use a cap, but you must use a high quality cap.
Our simple experiment.
one Friday afternoon,I decided to test this very same question.
I mustered up three different brand caps.
SUNTAN 2000u 25V
Nichon 2200V 10V
some noname rubbish
Leakage test:
Simply I charged them all to 5V and left them on the bench disconnected from everything for the weekend.
Results:
the no name and SUNTAN caps were close to 1 volt. internal resistance has discharged the cap.
the Nichon was still over 4V. to lose 1 V in 2 days, 2000uF is not enough for this question.
So Yes a super cap would work if its a good quality brand. but they suck current hard.
Don't charge it from the pin. I suggest a diode from the 3V reg with 100R in series to reduce the current
Avoid any battery if possible,
I don't think that CR2032 series batteries are a danger to the airline industry since the delivery of current is very low, maximum 10-100mA roughly. depending on size
how many days do you want the cap to hold up the ram ?
In my last design, I used the biggest CR2032 for the RTC, it should run for 10 years without external power.
2018-01-14 1:25 PM
I would consider a series resistance to limit charging current when first powered on.
JW
2018-01-14 1:52 PM
We had a bright glow coming from a test board in 1985, it was a tantalum cap on fire.
We don't use tants for that reason alone.
2018-01-21 9:54 PM
Thank you for your answers.
After charging 3.3V, the systemclockconfig can't pass the LSE ready.
After removing the capacitor in the circuit, then it has passed this condition.
Then, I have connected it the VBAT pin again, it can't pass again.
2018-01-23 9:10 AM
I haven't found any solution yet, anybody has a solution?
2018-01-23 10:24 AM
can't pass the LSE ready.
Show code, where does it stuck?
JW
2018-01-23 2:26 PM
As long as you connect them differently than capacitors. You should not charge them.
By the way T J, testing lytics may not be so simple. They well may have high leakage at first. Especially if they are stored for a long time. You have to keep power on for a while..
2018-01-24 2:36 AM
After removing the capacitor, it can pass
HAL_RCC_OscConfig(&RCC_OscInitStruct), otherwise it can't.
void SystemClock_Config(void)
{RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;RCC_PeriphCLKInitTypeDef PeriphClkInit;/**Configure LSE Drive Capability
*/__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);/**Initializes the CPU, AHB and APB busses clocks
*/RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;RCC_OscInitStruct.LSEState = RCC_LSE_ON;RCC_OscInitStruct.MSIState = RCC_MSI_ON;RCC_OscInitStruct.MSICalibrationValue = 0;RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK){_Error_Handler(__FILE__, __LINE__);}/**Initializes the CPU, AHB and APB busses clocks
*/RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{_Error_Handler(__FILE__, __LINE__);}PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK){_Error_Handler(__FILE__, __LINE__);}/**Enables the Clock Security System
*/HAL_RCCEx_EnableLSECSS();/**Configure the main internal regulator output voltage
*/if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK){_Error_Handler(__FILE__, __LINE__);}/**Configure the Systick interrupt time
*/HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/**Enable MSI Auto calibration
*/HAL_RCCEx_EnableMSIPLLMode();/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}2018-01-24 10:09 AM
One big difference between a capacitor and a battery is that a battery has a nominally constant output voltage, whereas a capacitor's terminal voltage drops linearly to zero as it discharges.
Remember: Q = CV ...
2018-01-24 12:54 PM
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
Try high.
After removing the capacitor, it can pass
HAL_RCC_OscConfig(&RCC_OscInitStruct), otherwise it can't.
Please step through the HAL_RCC_OscConfig() and observe where particularly is the problem.
JW