STM32L432KC Nucleo GPIOA resets to 0xABFF FFEF instead of 0xABFF FFFF
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-12 2:38 PM
STM32L432KC Nucleo GPIOA resets to 0xABFF FFEF instead of 0xABFF FFFF
I can't write 0 to $4800 0000 [GPIOA_MODER]
Ports B and C behave as expected: the correct reset values and it is possible to write 0x0000 0000 to B and C.
How can I resolve this?
Or has GPIOA died?
Firmware version: V2J45M31
ST-LINK/V2-1
- Labels:
-
ST boards
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-23 7:43 AM
Hi @Karel ,
It looks like PA2 is configured as alternate function in your case.
Can you try the following:
- Use STM32CubeProgrammer to read GPIOA_MODER register
- Perform a mass erase it remains the same
- Try an ST-Link firmware upgrade if needed.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-23 8:11 AM - edited ‎2025-04-23 8:12 AM
works for me in VS code and CubeProgrammer. Same Firmware version.
bare metal assembly to switch the GPIO clock(s) on, nothing else:
_start:
ldr r0, =0x40021000
movs r1, #3
str r1, [r0, #0x4C]
KnarfB