cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L412: State of pin PB9 doesnt change, no matter the configuration

VKuma.7
Associate

Hello,

Thank you in advance for any answers and your time.

I am using STM32L412CBT6P for my application. There are 2 custom boards with the same part and the following problem exists in both of the boards. Also attached is the connections diagram to the MCU.

The problem: PB9 of the MCU is clamped at exactly 1.2V despite of any configuration. The configuration I tried include output high, low, open drain; input - no push pull, pull up and pull down; external interrupt. I also tried putting an external pull down and; lastly, I tried lifting the pin to not have any connection at all, but with no results whatsoever.

Even without any firmware the pin stays at 1.2V despite the reset state of GPIOs being input(?).

Any hint towards the solution would be appreciated.

Regards,

Vivek

11 REPLIES 11
TDK
Guru

Pin PB9 is pin 45. Pin 46 is VDD12, which is indeed clamped to 1.2V, or at least should be.

My guess is you will find the same issue with PB11 on your current board.

0693W000005AL57QAG.png 

Perhaps you want a STM32L412CBT6 chip instead. They have different pinouts.

If you feel a post has answered your question, please click "Accept as Solution".
VKuma.7
Associate

Hello,

Thank you for the reply.

You are right about STM32L412CBT6 being the desired device and not STM32L412CBT6P.

They have the same datasheet (DS12469 Rev 7) and they have not mentioned the SMPS variant for the LQFP-48 footprint. Compared to proper details and pinout diagrams (page 50 - 54) and pin details table (page 56 onwards) for all the other versions with different pinouts.

Now I have manufactured about 100 boards with the wrong controller and it would all be a loss or require a lot off manual patch work.

Regards,

Vivek

MFass.1
Associate

Hi,

I fell into the same trap when I tried to use STM32L412CBT6. Here I'm using PB11 like USART3_RX.

In the datasheet (DS12469 Rev 8) there aren't explicit differences between versions with and without P for the LQFP48 package.

CubeIDE has the same problem, there aren't any pinout differences between these two kinds of Part Numbers.

Thanks.

TDK
Guru

> CubeIDE has the same problem, there aren't any pinout differences between these two kinds of Part Numbers.

Sure seem different to me in STM32CubeIDE:

0693W000006Ei1jQAC.png 

> In the datasheet (DS12469 Rev 8) there aren't explicit differences between versions with and without P for the LQFP48 package.

The datasheet is missing the SMPS LQFP48 package pinout, but it's there for the LQFP64 and others.

If you feel a post has answered your question, please click "Accept as Solution".

You are right.

I was choosing the device by the generic Part Number, that automatically selects the version without P.

I didn't realize that was possible to choose the device by the reference.

My mistake. 

Thanks.

bobaruni
Associate II

I too have manufactured a batch of boards and none of them work for the same reason.

Which part was the board designed for, and which did you use to build them?

Right now with the shortage of parts a lot of less popular versions are available from secondary sources, need to be very careful about part numbers and suffixes.

The -P ones being particularly troublesome due to pins moving around or being eliminated.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Piranha
Chief II

After 2 years they finally added LQFP48 SMPS pinout in DS12469 Rev 9.

Thanks Tesla, the board was designed for STM32L412CBT6 but I manufactured a batch using STM32L412CBT6P thinking they are just a different packaging SKU as in tape and reel vs tray.

There are several variants of the L412CBT6 at Mouser and they all list 38 I/O for all of them which I now know not to be the case as 2 of those pins are used for the 1.2v supply in the P suffix.

Unfortunately my design used both of the supply pins as GPIO so it doesn't work, luckily I have been able to get some stock of the STM32L412CBT6.

An of course there is not a single mention of the STM32L412CBT6P or STM32L412CBT6 for that matter in the latest datasheet.