STM32L4 DMA read write multiple blocks problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-03 3:36 AM
Posted on August 03, 2017 at 12:36
I have a problem with DMA mode reading multiple blocks.
To simplify a problem i took an example from the
STM32Cube_FW_
L4_V1.8.0\Projects\STM32L476G_
EVAL\Applications\FatFs\FatFs_
uSD\ archive.
BSP_SD_ReadBlocks_DMA
is used.
Read blocks not worked good, it started to work after i separated rx and tx and added Init and Deinitto DMA each time that i use that channel.
The problem is witha write now. I can write only blocks that are less then 1k. from 1k to 4096 sometimes it can write and sometimes
f_writereturn 0x
It always fails to write blocks bigger then 4096, bsp_write_blocks always fails with MSD_ERROR .
The problem only in DMA mode, polling mode works great.
Note: this post was migrated and contained many threaded conversations, some content may be missing.
- Labels:
-
DMA
-
SDIO-SDMMC
-
STM32L4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-03 5:18 AM
With write using SDIO+DMA, one problem is that the DMA completes long before the SDIO FIFO clears, so using the DMA TC as a completion indicator is problematic. So after confirming DMA TC signals, you then need to watch the FIFO depth zero out.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-03 6:36 AM
Thank you for your fast reply.
Do you know which function should we use to check the FIFO empty state?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-03 10:11 AM
It will be the SDMMC_FIFOCNT register, you'll need to grep the library source to see how that is exposed/wrapped.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-23 5:01 AM
Hi,
Even I am facing problem when trying to read/write in DMA mode.
Rewritten call back functions in my c file and checking the card status also.
I am working on f4 disco EVAL.
Kirillov.Yaroslav
please let me know if you got read/write DMA working with one and multiple blocks.
Thanks,
Poonam
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-23 6:34 AM
He's using an L4, not an F4
STM32Cube_FW_F4_V1.19.0\Projects\STM32446E_EVAL\Applications\FatFs\FatFs_uSD_RTOS\Src\sd_diskio_dma.c
SDIO+DMA is workable on a number of F4 platforms
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-26 2:09 AM
Hi Clive,
You are right that SDIO+DMA is workable on a number of F4 platforms but I have following issue.
When I read/write single block in DMA mode without file system , it is working fine.
But When I am writing/ reading multiple blocks (1000) blocks in loop , I am not sure what exactly is happening.
I am writing and trying to read same data in buffer. That buffer (Rx), when I print, it is empty.
while(i++ < 1000)
{ txDone = 1; //printf(' Write_addr is 0x%x \n' ,addr); HAL_SD_WriteBlocks_DMA(&hsd, Tx, addr, 1); while(txDone == 0 ){} //it will be set in call back function while(HAL_SD_GetCardState(&hsd) != HAL_SD_CARD_TRANSFER){} addr += 0x200; }while(i++ < 1000)
{ rxDone = 1; HAL_SD_ReadBlocks_DMA(&hsd, Rx, read_addr, 1); while(rxDone == 0 ){} // it will be set in callback function while(HAL_SD_GetCardState(&hsd) != HAL_SD_CARD_TRANSFER){} read_addr += 0x200; printf('RX is %s \n', Rx); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-26 7:46 AM
How is rxDone/txDone going to work here? Apt to immediately drop through.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-26 8:10 AM
Hi Clive,
Following are my callback functions where I am using these rxDone/txDone.
void HAL_SD_TxCpltCallback(SD_HandleTypeDef *hsd)
{ if (hsd->Instance==SDIO) { txDone = 0; }}void HAL_SD_RxCpltCallback(SD_HandleTypeDef *hsd)
{ if (hsd->Instance==SDIO) { rxDone = 0; }}Also,
I am able to write 1000- blocks with DMA write by adding following lines of code in HAL_SD_WriteBlocks_DMA()
/* Clear all the static flags */
__HAL_SD_CLEAR_FLAG(hsd, SDIO_STATIC_FLAGS); hsd->State = HAL_SD_STATE_READY;Have also added these lines of code in HAL_SD_ReadBlocks_DMA(), but its working only in debug mode.
Working on HAL_SD_ReadBlocks_DMA () to read multiple blocks.
Thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-26 9:17 AM
The logic is broken.
Up vote any posts that you find helpful, it shows what's working..