cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151VE ADC in sequence reads higher value for the 1st rank

Pavel Krupets
Associate III

ADC consistently reads higher value for any channel which is 1st in the sequence. If I query this channel 2nd time as rank 2 (immediately after high value) then it reads normal value. Value is high by about 10%.

Tested on stable input many-many times.

Is this normal?

3 REPLIES 3
Uwe Bonnes
Principal III

It is normal if you use too small sampling times.

Pavel Krupets
Associate III

Thank you!

It is a kind of interesting that while reading 24 channels in a sequence only 1st one gets it wrong. 🙂

Pavel Krupets
Associate III

This also reproduces if I use 16 MHz ADC clock with 16 cycles sampling time (original problem had 4 cycles).

It is not a big deal though as sampling the same channel again fixes the problem.