2019-03-13 1:32 AM
ADC consistently reads higher value for any channel which is 1st in the sequence. If I query this channel 2nd time as rank 2 (immediately after high value) then it reads normal value. Value is high by about 10%.
Tested on stable input many-many times.
Is this normal?
2019-03-13 5:39 AM
It is normal if you use too small sampling times.
2019-03-13 11:25 AM
Thank you!
It is a kind of interesting that while reading 24 channels in a sequence only 1st one gets it wrong. :)
2019-03-13 2:40 PM
This also reproduces if I use 16 MHz ADC clock with 16 cycles sampling time (original problem had 4 cycles).
It is not a big deal though as sampling the same channel again fixes the problem.