cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151RCT6 bsd

philippTT
Associate

Hello,

I need the BSD-File for STM32L151RCT6 for Boundary Scan. Does anyone know, where I can get it? In the recources section I can only find an older .zip file with bsd files for other processors.

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
ELABI.1
ST Employee

Hi @philippTT 

Please find attached the requested BSDL files.

The file STM32L151RCT6 is already published on the web under the name STM32L1_436_LQFP64.

Thanks.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Andrew Neil
Evangelist III

Hi,

I can't find the correct Id-Code in the provided Files. Do I have to go with another one?

The Id Code of the processor, that I have to test is: 6427041, so it should be 0110001000010001 in the part number and I can't find a corresponding bsd-file.

ELABI.1
ST Employee

Hi @philippTT 

Please find attached the requested BSDL files.

The file STM32L151RCT6 is already published on the web under the name STM32L1_436_LQFP64.

Thanks.

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.