cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L073RZT6 UART Stops responding after power-on, reset fixes issue

IHarg.1
Associate III

Hello,

I am working with a custom board communicating via USB-2-USART IC (FT234XD-R). Upon power up, the board operates as expected. I can communicate with the device . After some time--usually 60sec or so, but not perfectly periodic-- the device will stop responding. Using a logic analyzer, it shows the FT234 is still sending data to the chip, but the chip is not responding.The graph below shows a power up, communications start, MCU stops responding and reset button restores COMS indefinitely. I have left the board running for 24hrs and do not see the same issue after reset.

IHarg1_3-1703097549948.png

Using the hardware reset button on the board, I can reset the MCU and no longer have any issues. A few debugging techniques I have tried so far:

  1. Debug mode w/ break points
  2. Setting an LED flash if UART config changes or breakout of main loop
  3. Printf or LED flash within the HAL lib error function void Error_Handler(void)

Current band-aid

Setting the independent watchdog fixes the issue, but I would like the resolve, rather than band-aid, the issue.

Background information

STMCUBE v 1.14

USART2 with RX and TX both using the DMA on different channels.

Configuration

IHarg1_0-1703096565834.png

Initialization

HAL_UARTEx_ReceiveToIdle_DMA(&huart2, (uint8_t*)uartRxBuffer, RX_BUFFER_MAX);

Callback structure

IHarg1_1-1703096660908.png

Debug mode w/ break points

When operating in debug mode I am unable to recreate the issue. Everything works as intended after power-up. I no longer have to click the hardware reset.

{

/* USER CODE BEGIN Error_Handler_Debug */

/* User can add his own implementation to report the HAL error return state */

__disable_irq();

TIM21->CCR1 = 60000;

while (1)

{

 

}

/* USER CODE END Error_Handler_Debug */

}

Setting an LED flash if UART config changes or breakout of main loop

This debugging method did not show an relevant information. The UART would stop responding, but we never entered the error handler or broke out of the main loop.

 

Let me know if more information is needed. Thanks for stopping by!

 

Isaac.

6 REPLIES 6

Check that the UART isn't holding any sticky errors like noise, parity, framing, over-run, etc. Clear those errors if pending.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Karl Yamashita
Lead II

Assuming that HAL_UARTEx_RxEventCallback isn't being called anymore after a bit.

You don't check for HAL status when you call HAL_UARTEx_ReceiveToIdle_DMA. If it returns HAL_BUSY, thenRx  interrupts is not longer enabled. So you're pretty much dead in the water.

 

See this Wiki and project which shows how to set a flag in order to recover if HAL_UARTEx_ReceiveToIdle_DMA does return HAL_BUSY.

https://github.com/karlyamashita/Nucleo-G431RB_Three_UART/wiki

If you find my answers useful, click the accept button so that way others can see the solution.
IHarg.1
Associate III

Hello all,

Thank you for your responses. Update on data gathering. What complicates the issue is I can not recreate it when trying in debug mode, so I've had to set flags and visuals to see if certain blocks of code run.

Question 1: Could it be my code outside of the UART COMS?

Answer 1: When not communicating with the board. I do not see a reset, so thus the watchdog is getting pet and all is well. I do not believe there to be problematic code outside of the information I have presented. If the board were reset by the watch dog, we would see an anomaly int the heart beat pulse in red seen below.

IHarg1_0-1703109377838.png

Question 2(Tesla DeLorean :( UART isn't holding any sticky errors like noise, parity, framing, over-run, etc

Answer 2: I checked that the UART error callback is not called and checked the interrupt was enabled. (Watch dog is disabled now so I can glimpse into the issue) From the graph you can see that COMS start and everntually the MCU stops responding. In my UART error callback I turn off the heart beat light PWM, but notice that it never reaches that block of code from the graphs perspective.

IHarg1_2-1703110103501.png

IHarg1_1-1703110005216.png

Question 3(Karl Yamashita:( HAL_UARTEx_ReceiveToIdle_DMA returns busy & dead in the water

Answer 3:As a quick check if this would be the culprit, I put the HAL_UARTEx_ReceiveToIdle_DMA right in my main loop to be consistently re-initialized. From the graph, you can see that the issue still arises.

Great call out. I will be sure to add this redundancy checking in my code.

IHarg1_3-1703110505228.png

IHarg1_4-1703110690328.png

 

 

Please see response below.

Thanks for the comment! Please see the response below.

Yeah, what I'd want to see are the registers from the DMA and UART peripheral units in the failing, and non-failing conditions, so I could better understand the internal context, rather than observations at a pin level.

Print them out via a secondary debug channel, not screen shots in the debugger. Watch the reading DR/RDR or FIFOs has secondary effects on the status, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..