2024-09-28 08:29 PM
Previous post here didn't seem to get answered, so I thought I'd ask again.
Is there a way to execute code with the XIP framework, but not using the external SDRAM for instruction execution?
I'd like to use internal AHB or AXI Ram sections for code execution, and use the external ram for other purposes.
There doesn't seem to be any MX options or #defines in the XIP template to indicate this as an option.
I'm still digging through the code to have a better understanding of the system, but I'm not sure if this will be a fools errand if this configuration is not possible.
If there is a way to do this, if anyone can direct me to any documentation on the setup, that would be wonderful.
Thanks,
-Hal