STM32H7R3. SMPS and VCORE.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-30 01:49 AM
Hello
Can anybody explain how it is possible to power VCORE directly from SMPS output?
I see that SMPS have only two possible output voltages, 1.8V and 2.5V:
But VCORE accepts absolute maximum of 1.4V.
So how it is possible with LDO bypassed?
Best Regards
Solved! Go to Solution.
- Labels:
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-30 03:32 AM - edited ‎2025-01-30 03:32 AM
Depending on the mode you wish to work in,
you need to properly set the bits (SDHILEVEL, SMPSEXTHP, SDEN, LDOEN, BYPASS) found in Table 44. Supply Configuration Control in the Reference Manual RM0477
For the SDHILEVEL bit, which controls whether the SMPS outputs 1.8V or 1.2V
- If this bit is set to 0 -> 1.2V
- If it is set to 1 -> 1.8V
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-30 03:32 AM - edited ‎2025-01-30 03:32 AM
Depending on the mode you wish to work in,
you need to properly set the bits (SDHILEVEL, SMPSEXTHP, SDEN, LDOEN, BYPASS) found in Table 44. Supply Configuration Control in the Reference Manual RM0477
For the SDHILEVEL bit, which controls whether the SMPS outputs 1.8V or 1.2V
- If this bit is set to 0 -> 1.2V
- If it is set to 1 -> 1.8V
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-30 04:25 AM - edited ‎2025-01-30 04:26 AM
Thanks.
So there are two additional information, important for me:
1. SMPS may have different voltage than 1.8 / 2.5 V.
2. There are another power mode, not indicated in schematic: SMPS on, VCORE powered from SMPS but with LDO on.
Thanks for this.
Best regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-30 08:15 AM
When the LDO is on, it only powers the Vcore. You cannot power the Vcore with both the SMPS and the LDO at the same time.
Thanks.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-30 10:18 AM - edited ‎2025-01-30 10:24 AM
I mean the situation when VCORE is powered from SMPS thru LDO.
This mode is not listed here:
But it was mentioned here:
The closest mode is mode 3, when we externally make this connection:
But for some reason, You didn't include this mode in the documentation.