2024-08-29 03:03 AM
Hello, I am looking for the BSDL files for the processors of the STM32H757I-EVAL board and the STM32H755 processor. Thanks in advance!
Solved! Go to Solution.
2024-08-29 03:31 AM - edited 2024-08-29 03:32 AM
Sorry for the Mistake. I've correct it on the First replay. Here is the correct link:
https://www.st.com/resource/en/bsdl_model/stm32h7_bsdl.zip
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-29 03:14 AM - edited 2024-08-29 03:30 AM
Hello @MFrie.7
All BSDL files for STM32H7 MCUs are available here:
STM32H747_757_TFBGA240.bsd is the one for the MCU included on the STM32H757I-EVAL.
For the STM32H55 MCU, you need to check which package you are using, and you will find the suitable file for your MCU.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-29 03:28 AM
Hello STTwo-32
Thanks for the quick reply. I'm a bit confused from the link you sent. I get .svd files with it, but I need the .bsd files.
Best regards
2024-08-29 03:31 AM - edited 2024-08-29 03:32 AM
Sorry for the Mistake. I've correct it on the First replay. Here is the correct link:
https://www.st.com/resource/en/bsdl_model/stm32h7_bsdl.zip
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.