cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H757-IEVAL and STM32H755 BSDL File

MFrie.7
Associate II

Hello, I am looking for the BSDL files for the processors of the STM32H757I-EVAL board and the STM32H755 processor. Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions

Sorry for the Mistake. I've correct it on the First replay. Here is the correct link:

https://www.st.com/resource/en/bsdl_model/stm32h7_bsdl.zip

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @MFrie.7 

All BSDL files for STM32H7 MCUs are available here:

STM32H747_757_TFBGA240.bsd is the one for the MCU included on the STM32H757I-EVAL.

For the STM32H55 MCU, you need to check which package you are using, and you will find the suitable file for your MCU.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello STTwo-32

Thanks for the quick reply. I'm a bit confused from the link you sent. I get .svd files with it, but I need the .bsd files.

Best regards

Sorry for the Mistake. I've correct it on the First replay. Here is the correct link:

https://www.st.com/resource/en/bsdl_model/stm32h7_bsdl.zip

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.