2023-10-11 9:32 AM - edited 2023-10-11 9:34 AM
Hello everyone,
I open a new topic since my issue seems to be characterizing only my application.
I have implemented what I consider a rather stable lwIP - ModbusTCP/IP on a proprietary application using STM32H755 microcontroller. As long as I work with one board only, everything works fine, both ping and data exchange. As soon as I connect a second identical board but with different IP (verified), only one of the two allows to ping or exchange data(tried to do it together, separately, everything i could think of). If I stop the connection to the first CPU, even disconnecting it's cable, the communication returns to the previous working condition (ok). Then I tried to ping the two CPUs with two different laptops simultanously and the same thing happens, ping works only on one board at a time.
If I try to ping the same board while transferring data (SW too emulating Modbus Client) it works just fine.
To me it seems like a very long handshake, like the link is never left idle for the other participants to complete their operations. I must say that I never even tried to establish multiple connections at once with a laptop to different devices so I didn't think any of it at first and I'm still not sure if it's normal or not, even if I would say not.
Have you ever encountered the same issue while developing on stm32 platforms? Do yuou know any additional test I might perform to address this issue? Or maybe in which direction to look at for more insights? Could it be an issue in my Modbus TCP/IP protocol (just so you know, it's OS free and running it's main functions through callbacks)?
Thank you all in advance,
Zack
2023-10-11 10:52 AM
@ all
I just went through a self-brainstorming and though about the fact that actually there is one thing that might cause issues on the matter: that is MAC address. CubeMX assigns always the same one to every device.
Tomorrow is testing day, I'll post if it has solved the issue reported.
2023-10-11 2:47 PM
We use something like this to auto-generate MAC addresses for quick testing.
#include <stm32h7xx_hal.h>
// Generate MAC address from STM32 "unique ID":
// byte [1]=02 (locally managed), [1]=arg, [2..5] from "unique ID"[0]
void BSP_get_MAC_addr(uint8_t addr[6], uint8_t a1)
{
addr[0] = 0x02;
addr[1] = a1;
uint32_t u = HAL_GetUIDw0();
__UNALIGNED_UINT32_WRITE(&addr[2], u);
}
2023-10-12 2:07 AM
Yes, the issue was the MAC address as expected.
Unfortunately the solution provided by @Pavel A. is not working in my case since ICache is enabled and I should set MPUs. I must dedicate some more time to the topic, I don't have the required knowledge to proceed in that direction. I'll just use a parameter coming from EE to set it for the time being.
Thanks for the help!
2023-10-12 5:29 PM
The device ID has many bits that are likely to be the same for a devices of the same batch. It is much better to compute a 32-bit CRC on all 96 bits of the device ID and use those 4 bytes for the MAC address.
2023-10-12 10:24 PM
For now (still in dev stage) I'm doing it almost like @Pavel A. :
/* MAC adress: get some bytes from unique STM32 ID at UID_BASE */
u8MacAddr[0] = 0x01;
u8MacAddr[1] = 0x23;
u8MacAddr[2] = (uint8_t)(0x000000FF & (HAL_GetUIDw0() >> 0));
u8MacAddr[3] = (uint8_t)(0x000000FF & (HAL_GetUIDw0() >> 16));
u8MacAddr[4] = (uint8_t)(0x000000FF & (HAL_GetUIDw1() >> 0));
u8MacAddr[5] = (uint8_t)(0x000000FF & (HAL_GetUIDw2() >> 24));
But there's still the option to edit the MAC via UART and store and load it from SPI flash.
But @Piranha 's idea with the CRC sounds even better, I'll take a look at that.
2023-10-12 10:56 PM - edited 2023-10-15 10:44 PM
We use the I2C EEPROM 24AA025E48 from Microchip, which comes with an official pre-programmed MAC address in a read-only section of the memory.
2023-10-19 7:27 PM
Also change the value of the first byte to 0x02 or something else with that second bit set so that it makes a locally administered address. The 0x01 bit makes a group (multicast/broadcast) address.
2023-10-19 9:57 PM
Wow, never heard of that!
For the first 2 bytes, in my current development, I'm using actually some other "constant" with 0xE as lower nibble, don't know why I changed that when I copied that here.
But good to know anyway, thanks!
2023-10-29 3:14 AM
Hello everyone,
I actually had the cance to test on a nucleo board configured with a stm32H755 MCU, without any cache configuration enabled but I wasn't able to read any UID data.
According to RM0399 pag 3510, the UID base address is 0x1FF1 E800 on, but if i try to read the content with this function:
__STATIC_INLINE uint32_t LL_GetUID_Word0(void)
{
return (uint32_t)(READ_REG(*((uint32_t *)UID_BASE_ADDRESS)));
}
Provided on other threads here, it doesn't seem to work, I get Hard Faults every time.
Do you have any idea why is that?
Thanks in advance.
Zaack