2023-12-06 7:22 AM
Hi everyone,
I try to impement the LwIP Stack on my NUCLEO-H755ZI-Q Evaluation Board. I want to use the M4 core for the ethernet communication.
Unfortunately it results always in a StackOverflowHook if I connet with "Hercules" TCP Client and send a string.
I have configured the stack as described under https://github.com/stm32-hotspot/STM32H7-LwIP-Examples/tree/v1.2_ide_v1.9.0/STM32H745_Nucleo_M4_ETH.
The adapted LinkerScript "STM32H755ZITX_FLASH.ld" see below.
My TCPServer implementation tcpServerRAW.c is from https://controllerstech.com/stm32-ethernet-4-tcp-server/.
I attached my .ioc fiile and a video of the Stackoverflow error.
Maybe there is a configuration mistake?
Thank you.
** File : LinkerScript.ld
...
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08100000, LENGTH = 1024K
/* ETH_CODE: split memory to data and ethernet buffers */
RAM (xrw) : ORIGIN = 0x10000000, LENGTH = 128K /* ETH_CODE *
ETH_RAM (xrw) : ORIGIN = 0x10020000, LENGTH = 160K /* ETH_CODE *
MTI_SRAM (xrw) : ORIGIN = 0x38008000, LENGTH = 32K /* MTI: Shared Memory Bereich halber SRAM4 */
}
/* MTI: Shared Memory Bereich */
__MTI_SRAM_region_M4_start__ = ORIGIN(MTI_SRAM);
__MTI_SRAM_region_M7_start__ = ORIGIN(MTI_SRAM) + 1024;
__MTI_SRAM_region_end__ = ORIGIN(MTI_SRAM) + LENGTH(MTI_SRAM);
...
/* ETH_CODE: add placement of DMA descriptors and RX buffers */
.lwip_sec (NOLOAD) :
{
. = ABSOLUTE(0x10040000); /* 0x10040000 */
*(.RxDecripSection)
. = ABSOLUTE(0x10040060); /* 0x10040060 */
*(.TxDecripSection)
. = ABSOLUTE(0x10040200); /* 0x10040200 */
*(.Rx_PoolSection)
} >ETH_RAM
/* ETH_CODE: end */
...
}
Solved! Go to Solution.
2023-12-12 10:48 PM
After further attempts, I have now reached an initial working state where the uC does not crash. I sent more than 2,000,000 TCP/IP frames.
I am using STM32CubeIDE 1.9 and STM32Cube FW_H7 V1.10.0. The LWIP stack will probably also work in the latest STM32CubeIDE 1.13.1, with STM32Cube_FW_H7_V1.11.1.
2023-12-06 8:36 AM
Hello @Martin42
Check this FreeRTOS - stacks and stack overflow checking
It should be helpful
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-07 2:09 AM - edited 2023-12-07 5:47 AM
Hi,
thank you for the link to https://www.freertos.org/Stacks-and-stack-overflow-checking.html.
I have already implemented the vApplicationStackOverflowHook. In the attached video you can see the implemented function vApplicationStackOverflowHook() and how the program ends there.
I also monitored the stack size of each task with STM32CubeMonitor with the function https://www.freertos.org/uxTaskGetStackHighWaterMark.html. The stack size is for each task always the same size.
I have also added the configuration.
Maybe someone here can see at first glance what was configured incorrectly.
FreeRTOS M4 Configuration
LWIP Configuration
Also if I use the LWIP without FreeRTOS there is someting wrong...
2023-12-07 11:58 PM - edited 2023-12-08 12:45 AM
Hi,
I found a topic with "Downgrade to version 1.9 works well. Ethernet on the M4 core on version 1.10 is not working".
I use STM32CubeIDE 1.13.1 and Firmware Package V1.11.1
Is there still a problem there?
2023-12-11 1:14 AM - edited 2023-12-11 1:16 AM
Hello @Martin42
Thank you for reporting this issue.
I will check this issue internally and get back to you ASAP.
The issue is more likely
SCB_InvalidateDCache_by_Addr
is used for CM4. Could you confirm please?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-11 1:23 AM
Hi @FBL ,
I commented it out in CM4\LWIP\Target\ethernetif.c like:
//SCB_InvalidateDCache_by_Addr((uint32_t *)buff, Length); // NA
2023-12-11 5:57 AM
Hello,
after spending several hours trying the versions of the STMCubeIDE (1.6.1, 1.9.0, 1.13.1) with various combinations of the STM32Cube FW_H7 (V1.9.0, V1.9.1, V1.10.0, V1.11.0), I come to the conclusion that the application implementation is probably causing the problem.
/* Handle the incoming TCP Data */
static void tcp_server_handle (struct tcp_pcb *tpcb, struct tcp_server_struct *es)
{
struct tcp_server_struct *esTx;
/* allocate structure es to maintain tcp connection information */
esTx = (struct tcp_server_struct *)mem_malloc(sizeof(struct tcp_server_struct));
/* get the Remote IP */
ip4_addr_t inIP = tpcb->remote_ip;
uint16_t inPort = tpcb->remote_port;
/* Extract the IP */
char *remIP = ipaddr_ntoa(&inIP);
esTx->state = es->state;
esTx->pcb = es->pcb;
esTx->p = es->p;
char buf[100];
memset (buf, '\0', 100);
strncpy(buf, (char *)es->p->payload, es->p->tot_len);
strcat (buf, "+ Hello from TCP SERVER\n");
esTx->p->payload = (void *)buf;
esTx->p->tot_len = (es->p->tot_len - es->p->len) + strlen (buf);
esTx->p->len = strlen (buf);
tcp_server_send(tpcb, esTx);
pbuf_free(es->p);
mem_free(esTx);
}
Incorrect memory access can also be seen in the example video from ControllersTech https://youtu.be/olYTNjM2kwE?t=598. I thought it was because of the LWIP version.
I adapted the function to write to the same memory as the received data. So far this has been working without any problems.
static void tcp_server_handle (struct tcp_pcb *tpcb, struct tcp_server_struct *es)
{
char a[] = "abcdefghijklmnopqrstuvwxyzABCDEFGHIJKLMNOPQRSTUVWXYZ";
uint8_t ui8_loop;
static uint8_t ui8_switcher = 0;
uint8_t *pui8_payload;
pui8_payload = es->p->payload;
for(ui8_loop = 0; ui8_loop < (es->p->len - 1); ui8_loop++)
{
*pui8_payload = a[(ui8_loop + ui8_switcher) % ((sizeof(a)/sizeof(a[0])))];
pui8_payload++;
}
*pui8_payload = '\n';
ui8_switcher++;
tcp_server_send(tpcb, es);
}
I have attached the original tcpServerRAW.c.
Is there a simple example of a TCP/IP or UDP client-server implementation?
2023-12-12 10:48 PM
After further attempts, I have now reached an initial working state where the uC does not crash. I sent more than 2,000,000 TCP/IP frames.
I am using STM32CubeIDE 1.9 and STM32Cube FW_H7 V1.10.0. The LWIP stack will probably also work in the latest STM32CubeIDE 1.13.1, with STM32Cube_FW_H7_V1.11.1.