Skip to main content
halbeeee
Associate II
February 13, 2024
Question

STM32H755, is the clock too slow?

  • February 13, 2024
  • 32 replies
  • 16705 views

Hello everyone, I'm working on an STM32H755BI (industrial temperature range), and i'm quite disappointed by the maximum clock reachable from the system.

halbeeee_0-1707818384608.png

As can be seen, the MCU can reach up to 480MHz in the core M7 and 240MHz in the core M4.

After months of develpment, a firmware package update blocked me the VOS0 and VOS1, and in fact reading the user manual those modes are unavailable on my package, so i reduced to 300MHz and 150MHz

halbeeee_1-1707818577885.png

Today, with an update of cube MX, this error appeared in the clock tree:

halbeeee_2-1707818662175.png

And in fact by reading the datasheet APB4 is limited to 100MHz.

halbeeee_3-1707818726301.png

Reducing APB4 to 100MHZ could not be a big deal, but the real problem is that considering the clock distribution in the previous image the clock of the APB4 is the same clock of the M4 (CPU2).

 

Does this means that i bought a 480+240MHz and i'm forced to use it at 300+100 after more than a year of development?

This topic has been closed for replies.

32 replies

STOne-32
ST Technical Moderator
February 13, 2024

Dear @halbeeee ,

 

We have a specific application Note that explains the STM32H7 MCU Life time STM32H7 Series lifetime estimates - Application note : AN5337, depending on the Operation ratio of RUN/Low power modes and also Temperature .

Let me know how I can help you on your particular case to optimize it further.

Cheers,

STOne-32

halbeeee
halbeeeeAuthor
Associate II
February 13, 2024

Sorry, but i didn't get the point of your comment. How can my problem and the application note you posted be related?

STOne-32
ST Technical Moderator
February 13, 2024

It has a direct link on the maximum Frequency of the CPU and on the VOSx depending on the temperature.  In order to understand correctly your application use case, do you know what is the expected operating temperature ? For instance to reach 450MHz for M7 , VOS0 is a must , however limited to junction temperature up to 105 degrees Celsius.

TDK
February 13, 2024

Interesting.

The reference manual says it can do 480 MHz. It would be odd for the datasheet to have such a large error. The H745/H755 has been out for a while and is clearly advertised as 480 MHz capable. I would be surprised if it were only capable of 300 MHz.

The CubeMX folks tend to follow the datasheet, so it's not surprising that CubeMX flags the error.

The restriction seems to only be listed in that one figure. In many other places in the manual, it says CPU2 can run at 240 MHz, so that's not very consistent.

On the other hand, there is this note in the datasheet which suggests the change was intentional:

TDK_0-1707832122798.png

Nothing relevant in errata sheet.

Perhaps @STOne-32 can look a little more closely at this.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
February 13, 2024

Not sure the plumbing is consistent with how it used to be.

APB4 used to be fractional from the AHB clock (M4 CPU), so M7 400 MHz, AHB 200 MHz, APB4 100 MHz.

Should be possible to get 150 MHz M4, with 75 MHz APB4 using the same relationships.

I suspect the paper relates to electromigration exacerbated by speed and temperature. 

As I recollect the early H7's could hit >500 MHz in nominal conditions, vs 400 MHz spec, later revised upward to the 480 MHz on the V-Step

/**
 * @brief System Clock Configuration
 * The system Clock is configured as follow :
 * System Clock source = PLL (HSE BYPASS)
 * SYSCLK(Hz) = 400000000 (CPU Clock)
 * HCLK(Hz) = 200000000 (Cortex-M4 CPU, Bus matrix Clocks)
 * AHB Prescaler = 2
 * D1 APB3 Prescaler = 2 (APB3 Clock 100MHz)
 * D2 APB1 Prescaler = 2 (APB1 Clock 100MHz)
 * D2 APB2 Prescaler = 2 (APB2 Clock 100MHz)
 * D3 APB4 Prescaler = 2 (APB4 Clock 100MHz)
 * HSE Frequency(Hz) = 8000000
 * PLL_M = 4
 * PLL_N = 400
 * PLL_P = 2
 * PLL_Q = 4
 * PLL_R = 2
 * VDD(V) = 3.3
 * Flash Latency(WS) = 4
 * @PAram None
 * @retval None
 */
static void SystemClock_Config(void)
{
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 HAL_StatusTypeDef ret = HAL_OK;

 /*!< Supply configuration update enable */
 HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);

 /* The voltage scaling allows optimizing the power consumption when the device is
 clocked below the maximum system frequency, to update the voltage scaling value
 regarding system frequency refer to product datasheet. */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /* Enable HSE Oscillator and activate PLL with HSE as source */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
 RCC_OscInitStruct.HSIState = RCC_HSI_OFF;
 RCC_OscInitStruct.CSIState = RCC_CSI_OFF;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 400;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLQ = 4;

 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
 ret = HAL_RCC_OscConfig(&RCC_OscInitStruct);
 if(ret != HAL_OK)
 {
 Error_Handler();
 }

/* Select PLL as system clock source and configure bus clocks dividers */
 RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_D1PCLK1 | RCC_CLOCKTYPE_PCLK1 | \
 RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1);

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
 ret = HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4);
 if(ret != HAL_OK)
 {
 Error_Handler();
 }

 /*
 Note : The activation of the I/O Compensation Cell is recommended with communication interfaces
 (GPIO, SPI, FMC, QSPI ...) when operating at high frequencies(please refer to product datasheet)
 The I/O Compensation Cell activation procedure requires :
 - The activation of the CSI clock
 - The activation of the SYSCFG clock
 - Enabling the I/O Compensation Cell : setting bit[0] of register SYSCFG_CCCSR

 To do this please uncomment the following code
 */

 /*
 __HAL_RCC_CSI_ENABLE() ;

 __HAL_RCC_SYSCFG_CLK_ENABLE() ;

 HAL_EnableCompensationCell();
 */
}

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
halbeeee
halbeeeeAuthor
Associate II
February 13, 2024

@TDK Thank you for the reply. The maximum clock was reduced to 300MHz with the FW package 1.11.0 if i'm not wrong. But the datasheet confirms this maximum value of 300MHz and there is nothing to do. The reliability is a crucial requirements so i have to follow the requirements.

I also think that your pointed note refers to VOS3 (or at least i hope, since FCPU2 of 150MHz is allowed by cube)

 

@STOne-32 My problem is not the reduction from 480 to 300 MHz due to the VOSx settings, but the new limit in the APHB that blocks the CPU2 from reaching frequencies allowed by the current VOSx settings, limiting it from a theoretical 240Hz to a maximum of 100MHz.

Tesla DeLorean
Guru
February 13, 2024

>>I also think that your pointed note refers to VOS3 (or at least i hope, since FCPU2 of 150MHz is allowed by cube)

That would be my read of it too.

I suspect CubeMX is applying VOS3 rules, not VOS2 rules. The gearing would look to permit 300+150 or 200+200

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
February 13, 2024

APB4 != AHB4

The M4 MCU runs at AHB4, the peripheral bus runs from APB4 at 100 MHz or below

h7ahb4apb4.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
halbeeee
halbeeeeAuthor
Associate II
February 13, 2024

Yes you are right, I confused AHB4 and APB4 but this not change the fact that CubeMX don't allow me to apply 150MHz, which now is also a value that can be used according to the datasheet.

Is a kind of bug? Or a limit?

Tesla DeLorean
Guru
February 13, 2024

Me thinks it's a bug..

But I don't use CubeMX to build my clock trees.

The limits on the M4 are going to be critical path related in this context, running the transistors at 300 MHz isn't going make them run any hotter on the M7 vs M4 side of the die.

I've got Cortex-M3's running at 384 MHz on other processes, admittedly I don't have the FPU-S to contend with, but still.

Honestly I'd like to see a lot better analysis of where ALL these limitations are coming from. And what critical paths have been identified.

For example are there good reasons why 300+300, 250+250 or 240+240, etc aren't actually workable?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
February 13, 2024

>>Does this means that i bought a 480+240MHz and i'm forced to use it at 300+100 after more than a year of development?

What did the Data Sheet say about VOS2/VOS3 wrt Industrial Temp ranges when you started? Attach THAT document.

Probably 300+150 or 200+200 workable from current reading.

Or that you could derate and change gearing depending on temperature?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
February 13, 2024

@Tesla DeLorean You are likely correct that the figure is from before the max frequency was bumped from 400 MHz to 480 MHz. Figure would be consistent with 400 MHz. Good catch on APB vs AHB, I should have caught that.

All that acknowledged, the underlying question remains the same. Datasheet clearly indicates 480/240 is possible on that chip, yet CubeMX doesn't allow it.

Underlying problem seems to be CubeMX doesn't allow VOS0 or VOS1 to be selected on STM32H755. Unclear why, probably a bug, but I could be missing something. They simply don't appear as options. No such issues on STM32H745.

TDK_0-1707838571362.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
AScha.3
Super User
February 13, 2024

The basic "problem" is the allowed temperature range : -3  vs -6 , 125° vs 85° .

When 85° , 480/240MHz max., but at 125° 300/100MHz .

see

https://estore.st.com/en/stm32h755bit3-cpn.html

https://estore.st.com/en/stm32h755bit6-cpn.html

 

but wrong "promises" : > M7 core operates at up to 480 MHz ..< --- only for -T6 true !!!

AScha3_0-1707840190649.png

And with -T3 only VOS2 or 3 allowed...

If you feel a post has answered your question, please click on " Best Answer ".
Tesla DeLorean
Guru
February 13, 2024

>> but at 125° 300/100MHz .

Ok where do you see this? VOS2 = 300/150, VOS3 = 200/100

It's stuff like this that I find fantastically UNHELPFUL

h7bit3.jpg

What I'd find helpful is the critical paths in the M4 implementation, and the transistor performance expectations at 125C externally vs junction temperatures.

There are SURELY better options for derated speeds, even with the unhelpful dividers.

If we knew where ST believed the critical paths were it would be possible to characterize, observe failure, and provide adequate safety margins. Or clock gear based on  ADC_CHANNEL_TEMPSENSOR  (ADC_CHANNEL_18)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
February 13, 2024

Please check in CubeMX/IDE: RCC settings-> System parameters -> Product revision. Is it "V"?

Pavel A.
February 13, 2024

you know about the life time of the replicants ? 

Yeah, the life time of these poor folks was crippled deliberately. This was a parody to the popular conspiracy theory of these times, that makers of electric bulbs deliberately cripple the life time of their products. Hope this is not the case with ST ))

 

AScha.3
Super User
February 13, 2024

@Pavel A. , your great.

We discovered the conspiracy of the CPU manufacturers about the planned life time.

But we are in danger now - right?

If you feel a post has answered your question, please click on " Best Answer ".
STOne-32
ST Technical Moderator
February 13, 2024

Hi @AScha.3 @Pavel A. ,

This is  not new in the industrial applications where we push the product to full operating mode and at High temperatures. In recent years we are seeing many new design for solar applications to become more and more digital as exemple, so using our T3 profile becomes a mandatory choice for such devices.  And by the way, all of semiconductor manufacturers are providing similar applications notes and optimization techniques here is one example  https://www.ti.com/lit/an/sprabx4b/sprabx4b.pdf

Cheers,

STOne-32

Pavel A.
February 13, 2024

Whatever it's worth - the full Cube clock tree picture for both CPUs, with max. values everywhere. All arrows without a divisor box are not configurable (1:1). Yes, Cube is not documentation, the manuals prevail...

PavelA_0-1707866656225.png

 

@STOne-32 May your products be used only for solar and other peaceful things, and clear sky shine on the batteries.