cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753VIT6 PC2_C Pin

GOztu.1
Associate II

Hello, i am trying to use SPI2 on STM32H753VIT6 MCU using PD3 as Clock and PC2_C as MISO. Using the Hal libraries, i can generate clock on PD3 pin, and sensor answers me. But i dont get the sensor value on my software. Strange behaviour is, at its normal state i read 0xFF from PC2_C pin, but when i pull PC2_C to ground i can read 0x00. However i cannot read sensor data. When i changed the MISO pin to PB14 it worked. But i need PC2_C for my design. I have seen there have been people that had problems with PC2_C pin due to it being analog pin i assume. But i dont see anything on errata sheet. How can i solve my problem?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions

You need to ensure you don't exceed 1mA as external load:

From the errata:

SofLit_0-1730817097640.png

+ In the datasheet:

SofLit_1-1730817221225.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

View solution in original post

8 REPLIES 8
GOztu.1
Associate II

Edit: SYSCFG_PMCR PC2_C value is 0.

SofLit
ST Employee

Hello,

Check first the Switch status of PC2_C: https://community.st.com/t5/stm32-mcus-products/stm32h7-pc2-c-and-pc3-c-gpio-not-working/m-p/738739

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

SYSCFG_PMCR registers PC2_C bit is 0. Also when i make SPI2 work at very low speed(20Kbit), i can see somewhat meaningful data but still sometimes it is wrong.

liaifat85
Senior III

Confirm that PC2_C is set to Input mode with a no-pull or pull-up configuration, as floating configurations on certain pins can lead to unstable readings.

What do you mean by Input mode? I am assuming you dont mean the value stated in MODER register because i have already stated that i am using PC2_C as SPI2_MISO pin so Alternative Function. Also, pin is configured as no pull up or pull down.

You need to ensure you don't exceed 1mA as external load:

From the errata:

SofLit_0-1730817097640.png

+ In the datasheet:

SofLit_1-1730817221225.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.
GOztu.1
Associate II

How can i make sure that MISO pin sunks less than 1mA of current?

You need to measure that current and at any time that should exceed 1mA PK-PK.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.