2019-09-12 04:21 AM
Hello,
In the STM32H753AI datasheet, there are footprint guidelines for all the packages, except for the UFBGA169 (see attached image).
Has anyone built a board with this package? Where did you find any info on this type of package?
Is there a database of ST footprints I can look at to find this info?
In a similar question, one of the answers led to AN4938 (Getting started with hardware dev....), but there is no specific package information there either...
Thanks in advance,
Yan
2019-09-12 01:06 PM
stm32l4a6 has a similar UFBGA169 package, and I see it's data-sheet has a recommended footprint for a single pad, which is more than you got in your data sheet. Maybe you could build something from that?
But I think this is something you will have to discuss with your pcb house.
I have resorted to stacked via-in-pad to route enough tracks out of an ST WLCSP100 package. Not cheap but I couldn't see how to get the inner tracks out.
Hope this helps,
Danish
2019-09-14 08:32 AM
Thanks for the answer, I saw that datasheet as well, just wanted to make sure that it's indeed the same package...
Yan
2019-09-27 09:35 AM
Hi @Yan Rosh ,
A request is tracked internally to add "UFBGA169 recommended footprint" for STM32H7 datasheets where this package is available.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.