2020-07-21 10:20 PM
If i enable the TimeOutActivation in the memorymappedmode then device hangup randomly. if i disable the TimeOutActivation then it work normally.
The code snippet as below :
QSPI_EnableMemoryMappedMode(QSPI_HandleTypeDef *hqspi)
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = 0xEB; // QUAD_INOUT_FAST_READ_DTR_CMD;
s_command.AddressMode = QSPI_ADDRESS_4_LINES;
s_command.AddressSize = QSPI_ADDRESS_24_BITS;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_4_LINES;
s_command.AlternateBytesSize = QSPI_ALTERNATE_BYTES_8_BITS;
s_command.AlternateBytes = 0xFF;
s_command.DataMode = QSPI_DATA_4_LINES;
s_command.DummyCycles = 4;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
/* Configure the memory mapped mode */
s_mem_mapped_cfg.TimeOutActivation = QSPI_TIMEOUT_COUNTER_ENABLE;
s_mem_mapped_cfg.TimeOutPeriod = 100;
I found this thread so i config the MPU as below but still won't work :
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = 0x0;
MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x87;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Configure the MPU attributes for the QSPI 32MB access */
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.BaseAddress = QSPI_BASE_ADDRESS; // address is 0x90000000
MPU_InitStruct.Size = MPU_REGION_SIZE_32MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
Any suggestion ..
2020-07-22 2:05 AM
Although not mentioned in the H750 errata sheet, this might be "2.4.3 Memory-mapped read operations may fail when timeout counter is
enabled." in ES0334 Rev 6 for F76xxx. The QSPI is quite similar across device families ...
2020-07-22 6:47 AM
Hi, I'm a colleague of Fema and currently investigating this issue together.
We're aware of the ERRATA of STM32F76x 2.4.3, but we have no clear idea about how to implement the workaround:
"Disable the timeout counter. To raise the chip select, perform an abort at the end of each memory-mapped operation."
The operation of memory-mapped mode is that we assign the s_command & s_mem_mapped_cfg, after that the read operations should be handled by the QSPI controller.
This project is battery-powered, and currently QSPI Flash consumes about 20% power of the whole device.
After timeout counter is enabled, QSPI consumption drops to 5%, but cannot last long before the device hang-up.
Any information on how to implement the workaround in ERRATA?