User Activity

Hi Everyone: we now have a problem running STM32H747XIH6 with Low-Power SDRAM (ISSI IS42VM32160E-75BLI) when the SDRAM clock is set to 100MHz, on our customized PCBA. I'd like to check if anyone has suggestions on how to debug.■ Description of the s...
Hi everyone, we have a problem using LPTIM4 PWM output on STM32H747I-DISCO when system enters STOP mode.In this project, I need two independent PWM outputs with fixed frequency to work, while system goes to STOP mode to save power. LPTIM1_OUT & LPTIM...
 We have some issue concerning STM32H747XIH6 design supplying 1.8V to VDD:■ Below are some design criterion of this project:A. VDD is designed to be 1.8V to save power.  A separate 3.3V source is used to supply VDD33USB & VDDA.B. USB HS function is r...
Kudos from