2024-07-12 12:17 AM
HELLO,
I have 2 issues
1. A bug report
CubeMx generated init code is wrong with LL lib
the marco config is not change from HAL to LL
2. I cannot enable dual ADC1/ADC2 continous conversion with dma, and at every tranfer finish trigger a intterupt
below is my code
/* ADC1 init function */
void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
LL_ADC_InitTypeDef ADC_InitStruct = {0};
LL_ADC_REG_InitTypeDef ADC_REG_InitStruct = {0};
LL_ADC_CommonInitTypeDef ADC_CommonInitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_ADC12);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOC);
/**ADC1 GPIO Configuration
PC4 ------> ADC1_INP4
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_4;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* ADC1 DMA Init */
/* ADC1 Init */
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_STREAM_4, LL_DMAMUX1_REQ_ADC1);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_4, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_4, LL_DMA_PRIORITY_VERYHIGH);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_4, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_4, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_4, LL_DMA_MEMORY_NOINCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_4, LL_DMA_PDATAALIGN_WORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_4, LL_DMA_MDATAALIGN_WORD);
LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_4);
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
LL_ADC_SetOverSamplingScope(ADC1, LL_ADC_OVS_DISABLE);
ADC_InitStruct.Resolution = LL_ADC_RESOLUTION_16B;
ADC_InitStruct.LowPowerMode = LL_ADC_LP_MODE_NONE;
LL_ADC_Init(ADC1, &ADC_InitStruct);
ADC_REG_InitStruct.TriggerSource = LL_ADC_REG_TRIG_SOFTWARE;
ADC_REG_InitStruct.SequencerLength = LL_ADC_REG_SEQ_SCAN_DISABLE;
ADC_REG_InitStruct.SequencerDiscont = DISABLE;
ADC_REG_InitStruct.ContinuousMode = LL_ADC_REG_CONV_CONTINUOUS;
ADC_REG_InitStruct.Overrun = LL_ADC_REG_OVR_DATA_OVERWRITTEN;
LL_ADC_REG_Init(ADC1, &ADC_REG_InitStruct);
ADC_CommonInitStruct.CommonClock = LL_ADC_CLOCK_ASYNC_DIV1;
ADC_CommonInitStruct.Multimode = LL_ADC_MULTI_DUAL_REG_SIMULT;
ADC_CommonInitStruct.MultiTwoSamplingDelay= LL_ADC_MULTI_TWOSMP_DELAY_2CYCLES_5;
LL_ADC_CommonInit(__LL_ADC_COMMON_INSTANCE(ADC1), &ADC_CommonInitStruct);
/* Disable ADC deep power down (enabled by default after reset state) */
LL_ADC_DisableDeepPowerDown(ADC1);
/* Enable ADC internal voltage regulator */
LL_ADC_EnableInternalRegulator(ADC1);
/* Delay for ADC internal voltage regulator stabilization. */
/* Compute number of CPU cycles to wait for, from delay in us. */
/* Note: Variable divided by 2 to compensate partially */
/* CPU processing cycles (depends on compilation optimization). */
/* Note: If system core clock frequency is below 200kHz, wait time */
/* is only a few CPU processing cycles. */
__IO uint32_t wait_loop_index;
wait_loop_index = ((LL_ADC_DELAY_INTERNAL_REGUL_STAB_US * (SystemCoreClock / (100000 * 2))) / 10);
while(wait_loop_index != 0)
{
wait_loop_index--;
}
/** Configure Regular Channel
*/
LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_1, LL_ADC_CHANNEL_4);
LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_CHANNEL_4, LL_ADC_SAMPLINGTIME_1CYCLE_5);
LL_ADC_SetChannelSingleDiff(ADC1, LL_ADC_CHANNEL_4, LL_ADC_SINGLE_ENDED);
/* USER CODE BEGIN ADC1_Init 2 */
LL_ADC_StartCalibration(ADC1,LL_ADC_CALIB_OFFSET,LL_ADC_SINGLE_ENDED);
//HAL_ADCEx_Calibration_Start(&hadc1,ADC_CALIB_OFFSET,ADC_SINGLE_ENDED); //ADC校验
/* USER CODE END ADC1_Init 2 */
}
/* ADC2 init function */
void MX_ADC2_Init(void)
{
/* USER CODE BEGIN ADC2_Init 0 */
/* USER CODE END ADC2_Init 0 */
LL_ADC_InitTypeDef ADC_InitStruct = {0};
LL_ADC_REG_InitTypeDef ADC_REG_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_ADC12);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOB);
/**ADC2 GPIO Configuration
PB1 ------> ADC2_INP5
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_1;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE BEGIN ADC2_Init 1 */
/* USER CODE END ADC2_Init 1 */
/** Common config
*/
LL_ADC_SetOverSamplingScope(ADC2, LL_ADC_OVS_DISABLE);
ADC_InitStruct.Resolution = LL_ADC_RESOLUTION_16B;
ADC_InitStruct.LowPowerMode = LL_ADC_LP_MODE_NONE;
LL_ADC_Init(ADC2, &ADC_InitStruct);
ADC_REG_InitStruct.SequencerLength = LL_ADC_REG_SEQ_SCAN_DISABLE;
ADC_REG_InitStruct.SequencerDiscont = DISABLE;
ADC_REG_InitStruct.ContinuousMode = LL_ADC_REG_CONV_CONTINUOUS;
ADC_REG_InitStruct.Overrun = LL_ADC_REG_OVR_DATA_OVERWRITTEN;
LL_ADC_REG_Init(ADC2, &ADC_REG_InitStruct);
/* Disable ADC deep power down (enabled by default after reset state) */
LL_ADC_DisableDeepPowerDown(ADC2);
/* Enable ADC internal voltage regulator */
LL_ADC_EnableInternalRegulator(ADC2);
/* Delay for ADC internal voltage regulator stabilization. */
/* Compute number of CPU cycles to wait for, from delay in us. */
/* Note: Variable divided by 2 to compensate partially */
/* CPU processing cycles (depends on compilation optimization). */
/* Note: If system core clock frequency is below 200kHz, wait time */
/* is only a few CPU processing cycles. */
__IO uint32_t wait_loop_index;
wait_loop_index = ((LL_ADC_DELAY_INTERNAL_REGUL_STAB_US * (SystemCoreClock / (100000 * 2))) / 10);
while(wait_loop_index != 0)
{
wait_loop_index--;
}
/** Configure Regular Channel
*/
LL_ADC_REG_SetSequencerRanks(ADC2, LL_ADC_REG_RANK_1, LL_ADC_CHANNEL_5);
LL_ADC_SetChannelSamplingTime(ADC2, LL_ADC_CHANNEL_5, LL_ADC_SAMPLINGTIME_1CYCLE_5);
LL_ADC_SetChannelSingleDiff(ADC2, LL_ADC_CHANNEL_5, LL_ADC_SINGLE_ENDED);
/* USER CODE BEGIN ADC2_Init 2 */
// HAL_ADCEx_Calibration_Start(&hadc2,ADC_CALIB_OFFSET,ADC_SINGLE_ENDED);
LL_ADC_StartCalibration(ADC2,LL_ADC_CALIB_OFFSET,LL_ADC_SINGLE_ENDED);
/* USER CODE END ADC2_Init 2 */
}
before is generated and below is added in main
LL_ADC_SetMultiDMATransfer(ADC12_COMMON,LL_ADC_MULTI_REG_DMA_EACH_ADC);
LL_DMA_SetDataLength(DMA1,LL_DMA_STREAM_4,4);
LL_DMA_ConfigAddresses(DMA1,LL_DMA_STREAM_4,(uint32_t)&(ADC12_COMMON->CDR),(uint32_t)&ADC_ConvertedValueDual[0],LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_ADC_Enable(ADC1);
LL_ADC_Enable(ADC2);
LL_ADC_EnableIT_OVR(ADC1);
LL_DMA_EnableIT_TC(DMA1,LL_DMA_STREAM_4);
LL_DMA_EnableBufferableTransfer(DMA1,LL_DMA_STREAM_4);
LL_DMA_EnableStream(DMA1,LL_DMA_STREAM_4);
expected behavior is the adc1/2 convert periodicly every 5cycles, and dma transfer data to &ADC_ConvertedValueDual[0]
then the DMA1_Stream4_IRQHandler() should've been triggered, however none of these are happened
if you have any suggestion please kindly reply
thx alot
Solved! Go to Solution.
2024-07-15 4:50 AM - edited 2024-07-15 4:50 AM
Hello @mize ,
How you configure and handle the DMA transfer complete interrupt ?
Did you start ADC conversions using LL_ADC_REG_StartConversion?
More details on the configuration of dual ADC mode and DMA provided in this section of RM0433.
2024-07-12 10:56 AM
Hello @mize ,
Please share your ioc file and the version used of CubeMx, this will help to reproduce the case.
2024-07-14 6:09 PM
2024-07-15 4:50 AM - edited 2024-07-15 4:50 AM
Hello @mize ,
How you configure and handle the DMA transfer complete interrupt ?
Did you start ADC conversions using LL_ADC_REG_StartConversion?
More details on the configuration of dual ADC mode and DMA provided in this section of RM0433.
2024-12-02 12:24 AM
Hello @mize ,
This issue is fixed in the latest release of STM32CubeMx v6.13.0.
Thank you for your contribution.