2023-08-07 5:43 AM
When i use uart8 for send data to arduino(add function in food recognition in the fp_vision_AI) ,when i use MX_USART8_UART_Init();(if i use // jump over this line the rest could run normally) the screen on the board get blocked(stopped),how could i check where i get wrong? anexo this parte of code.
Data i want to send as tipo of "%s %.0f%%"
sprintf(msg, "%s %.0f%%", NN_OUTPUT_CLASS_LIST[App_Context_Ptr->ranking[i]], *((float*)(App_Context_Ptr-;
HAL_UART_Transmit(&huart8,msg,10,1000);
2023-08-07 5:53 AM - edited 2023-08-07 5:56 AM
Try to format only integer variables (remove the float one for now). If this works, you are using the "small" C library variant that does not support printing floats. Then decide: either round the float number to a long and format it with %l (%ul) or select the C library variant with float print support (see the project settings and CubeIDE user manual).
Note also that the number of bytes to send for HAL_UART_Transmit (the 3rd arg) is not necessarily 10. Consider using snprintf instead of sprintf (especially at job interviews!)
2023-08-07 7:22 AM - edited 2023-08-07 7:27 AM
But the part i get block is MX_USART8_UART_Init() (this only show one objecto detective then do not change anymore, normally should change every 90ms),
static void MX_USART8_UART_Init(void) { huart8.Instance = UART8; huart8.Init.BaudRate = 115200; huart8.Init.WordLength = UART_WORDLENGTH_8B; huart8.Init.StopBits = UART_STOPBITS_1; huart8.Init.Parity = UART_PARITY_NONE; huart8.Init.Mode = UART_MODE_TX_RX; huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart8.Init.OverSampling = UART_OVERSAMPLING_16; huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart8, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart8, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart8) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART1_Init 2 */ /* USER CODE END USART1_Init 2 */ }
not the line of transmite.