cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745 Not Connecting - "No STM32 Target Found" Error

Harsh_Gajjalwar
Associate II

I am facing an issue where my STM32H7 board is not detected using STM32CubeProgrammer. I am using an STLINK-V3SET programmer, and the following error keeps appearing:

 

Error log:

17:04:59 : UR connection mode is defined with the HWrst reset mode
17:04:59 : ST-LINK SN : 0028001E3233510739363634
17:04:59 : ST-LINK FW : V3J13M4B5S1
17:04:59 : Board : STLINK-V3SET
17:04:59 : Voltage : 3.29V
17:04:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

17:06:59 : UR connection mode is defined with the HWrst reset mode
17:06:59 : ST-LINK SN : 0028001E3233510739363634
17:06:59 : ST-LINK FW : V3J13M4B5S1
17:06:59 : Board : STLINK-V3SET
17:06:59 : Voltage : 3.29V
17:06:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

 

Setup Details

  1. Board: STM32H745xi series
  2. Debugger: STLINK-V3SET
  3. Software: STM32CubeProgrammer 
  4. Voltage: 3.3V confirmed

 

Any help or suggestions would be greatly appreciated. Thanks in advance!

 
1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @Harsh_Gajjalwar ,

Which HW? ST board or custom board? if ST board, which one? if custom board what power supply are you setting SMPS or LDO?

Becarefull, if you didn't set the correct power supply which needs to be inline with your HW, you broken your board. So you need to recover it with this manipulation: How can I recover my STM32H7 board after facing a power configuration deadlock?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

3 REPLIES 3

@Harsh_Gajjalwar wrote:

 my STM32H7 board 


What board?

Please give details; also versions, etc: How to write your question to maximize your chances to find a solution

TDK
Guru

Has it ever worked or is this a brand new board/design? Are SWD/NRST pins connected? Show schematic, details.

If you feel a post has answered your question, please click "Accept as Solution".
SofLit
ST Employee

Hello @Harsh_Gajjalwar ,

Which HW? ST board or custom board? if ST board, which one? if custom board what power supply are you setting SMPS or LDO?

Becarefull, if you didn't set the correct power supply which needs to be inline with your HW, you broken your board. So you need to recover it with this manipulation: How can I recover my STM32H7 board after facing a power configuration deadlock?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.