STM32H745 FMC acces to external NOR with timing from RM0399 does not work (works only with burst, but not non-burst)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-23 4:54 AM
Hallo,
I'm using a STM32H745, that shall access an external NOR flash with the timing recommended by ST at the reference manual RM0399 on page 875. I did exactly reproduce this timing setting, but no access will be generated on the FMC pins.
When I change one single bit in this configuration (bit 8 = BURSTEN set to 1) the access works, but of course as BURST access. My intention is a non-burst access.
However, that proves that all other settings are basically ok, including pin configuration, providing clock to the FMC and generating read/write access to the FMC bank 1.
The issue can be reproduced on two ways:
First via debugger.
After configuring the pins and switching the FMC clock on, set the register BCR1 and BTR1 and generate access via memory browser.
Second with the following code:
{
// Peripheral clock enable
LL_RCC_SetFMCClockSource( LL_RCC_FMC_CLKSOURCE_HCLK );
LL_AHB3_GRP1_EnableClock( LL_AHB3_GRP1_PERIPH_FMC );
// Pin configuration
for( uint32_t i = 0; i < ARRAYSIZE(Pin_FMC); i++ )
{
Pin_FMC[i].Setup();
}
FMC_NORSRAM_TypeDef* const Dev = FMC_NORSRAM_DEVICE;
uint32_t const Bank = FMC_NORSRAM_BANK1;
__FMC_NORSRAM_DISABLE( Dev, Bank );
// Initialize SRAM control interface
MODIFY_REG( Dev->BTCR[Bank],
// --- field mask ---
// FMC_BCRx_MBKEN bank will be enabled later
FMC_BCRx_MUXEN |
FMC_BCRx_MTYP |
FMC_BCRx_MWID |
FMC_BCRx_FACCEN |
FMC_BCRx_BURSTEN |
FMC_BCRx_WAITPOL |
FMC_BCRx_WAITCFG |
FMC_BCRx_WREN |
FMC_BCRx_WAITEN |
FMC_BCRx_EXTMOD |
FMC_BCRx_ASYNCWAIT |
FMC_BCRx_CPSIZE |
FMC_BCRx_CBURSTRW |
FMC_BCR1_CCLKEN |
FMC_BCR1_WFDIS,
// FMC_BCR1_BMAP bank mapping default value is used
// FMC_BCR1_FMCEN FMC will be enabled later
// --- field values ---
FMC_DATA_ADDRESS_MUX_ENABLE |
FMC_MEMORY_TYPE_NOR |
FMC_NORSRAM_MEM_BUS_WIDTH_16 |
FMC_NORSRAM_FLASH_ACCESS_ENABLE |
FMC_BURST_ACCESS_MODE_ENABLE | // must be set to one, why?
FMC_WAIT_SIGNAL_POLARITY_LOW | // not used
FMC_WAIT_TIMING_BEFORE_WS | // don't care
FMC_WRITE_OPERATION_ENABLE |
FMC_WAIT_SIGNAL_DISABLE | // no effect in async mode
FMC_EXTENDED_MODE_DISABLE |
FMC_ASYNCHRONOUS_WAIT_DISABLE | // wait signal not used
FMC_PAGE_SIZE_NONE | // no effect in async mode
FMC_WRITE_BURST_DISABLE | // no effect in async mode
FMC_CONTINUOUS_CLOCK_SYNC_ONLY |
FMC_WRITE_FIFO_DISABLE
);
// Set SRAM timing parameters
MODIFY_REG( Dev->BTCR[Bank + 1],
FMC_BTRx_ADDSET | // --- field mask ---
FMC_BTRx_ADDHLD |
FMC_BTRx_DATAST |
FMC_BTRx_BUSTURN |
FMC_BTRx_CLKDIV |
FMC_BTRx_DATLAT |
FMC_BTRx_ACCMOD,
(2 << FMC_BTRx_ADDSET_Pos) | // --- field values ---
(1 << FMC_BTRx_ADDHLD_Pos) |
(1 << FMC_BTRx_DATAST_Pos) |
(1 << FMC_BTRx_BUSTURN_Pos) |
(3 << FMC_BTRx_CLKDIV_Pos) | // FMC_CLK period = 4 × fmc_ker_ck periods (240 MHz / 4 = 60 MHz)
(1 << FMC_BTRx_DATLAT_Pos) | // Data latency of 2 FMC_CLK clock cycles for first burst access
FMC_ACCESS_MODE_A
);
__FMC_NORSRAM_ENABLE( Dev, Bank );
// Enable FMC Peripheral
__FMC_ENABLE();
volatile uint16_t* const BankAddr = reinterpret_cast<volatile uint16_t*>(0x60000000);
volatile uint16_t r = *BankAddr; // generate read access
*BankAddr = 0xA5A5; // generate write access
}My questions:
Asynchronous access to NOR should work in non-burst mode as well as in burst mode.
Why does the non-burst example from ST not work?
How can a non-burst access achieved?
That you very much in indeed.
- Labels:
-
Documentation
-
FMC-FSMC
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-23 5:18 AM
Caching or MPU configuration of memory region?​
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-23 5:56 AM
Both caches are disabled and the MPU is not used.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-24 9:25 AM
I have now switched on the MPU and configured the NOR-memory space as device.
The BURST read and write access is working perfect, but when configuring the bank for non-burst (bit 8 = BURSTEN set to 0) no access happens.
The MPU is configured according to the NOR example FMC_NOR for STM32H743 from CubeIDE. I copied the MPU initialising sequence from this project:
{
HAL_MPU_Disable();
// Configure the MPU attributes as device for NOR
MPU_Region_InitTypeDef MPU_InitStruct =
{
.Enable = MPU_REGION_ENABLE,
.Number = MPU_REGION_NUMBER0,
.BaseAddress = reinterpret_cast<uint32_t>(BankAddr),
.Size = MPU_REGION_SIZE_16MB,
.SubRegionDisable = 0x00,
.TypeExtField = MPU_TEX_LEVEL0,
.AccessPermission = MPU_REGION_FULL_ACCESS,
.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE,
.IsShareable = MPU_ACCESS_SHAREABLE,
.IsCacheable = MPU_ACCESS_NOT_CACHEABLE,
.IsBufferable = MPU_ACCESS_BUFFERABLE
};
HAL_MPU_ConfigRegion( &MPU_InitStruct );
HAL_MPU_Enable( MPU_PRIVILEGED_DEFAULT );
}Note: The FMC_NOR example project for STM32H743 from CubeIDE is using the FMC in non-multiplexed mode where I have to use the FMC in multiplexed mode.