STM32H743 Stack and Heap
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-23 11:59 AM
Hi,
I have my scatter file defined thus:
// Scatter file
LR_IROM1 0x08000000 0x00200000 { ; load region size_region
ER_IROM1 0x08000000 0x00200000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM2 0x24000000 0x00080000 { ; RW data
.ANY (+RW +ZI)
}
RW_DMARxDscrTab 0x30040000 0x60 {
*(.RxDecripSection)
}
RW_DMATxDscrTab 0x30040060 0x140 {
*(.TxDecripSection)
}
RW_Rx_Buffb 0x30040200 0x1800 {
*(.RxArraySection)
}
}
The startup file defines the following:
// startup_xx.asm
Stack_Size EQU 0x8000 (32,768 -> 32k)
Heap_Size EQU 0x0F800 (63,488 -> 62k)
As per the RM;
RAM
------------------------------------------
0x20000000 - 0x2001FFFF DTCM-RAM <-- Stack & Heap is here (Size: 0x1ffff = 131071, 128kB)
0x20020000 - 0x23FFFFFF Reserved
0x24000000 - 0x2407FFFF AXI SRAM <-- Current IRAM2: (Size: 0x7ffff, 524287, 511kB)
0x24080000 - 0x2FFFFFFF Reserved
0x30000000 - 0x3001FFFF SRAM1 <-- (Size: 0x1ffff, 131,071, 128kB)
0x30020000 - 0x3003FFFF SRAM2 <-- (Size: 0x1ffff, 131,071, 128kB)
0x30040000 - 0x30047FFF SRAM3 <-- Current Rx/Tx Descriptors, Rx buffers (Size: 32767, 128kB)
0x30048000 - 0x37FFFFFF Reserved
0x38000000 - 0x3800FFFF SRAM4 <-- (Size: 0xffff, 65535, 64kB)
0x38010000 - 0x387FFFFF Reserved
0x38800000 - 0x38800FFF Backup SRAM <-- NVRAM (Size: 0xfff, 4095, 4kB)
0x38801000 - 0x3FFFFFFF Reserved
As per the RM, the stack and heap are located @0x20000000 (IRAM1), Size=128k
According to my scatter file:
IRAM2 (0x24000000) is used
So, does that really mean that the Stack and heap are now in IRAM2, Size=511k ?
Can someone clarify ?
Thanks,
Manu
- Labels:
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-23 1:20 PM
Look in your startup script to find out what gets loaded into the SP register. That's where the end of your stack is.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-23 1:51 PM
The startup script is defined thus:
Stack_Size EQU 0x8000
AREA STACK, NOINIT, READWRITE, ALIGN=3
Stack_Mem SPACE Stack_Size
__initial_sp
; <h> Heap Configuration
; <o> Heap Size (in Bytes) <0x0-0xFFFFFFFF:8>
; </h>
Heap_Size EQU 0x0F800
AREA HEAP, NOINIT, READWRITE, ALIGN=3
__heap_base
Heap_Mem SPACE Heap_Size
__heap_limit
PRESERVE8
THUMB
; Vector Table Mapped to Address 0 at Reset
..
..
..
; end of vector tables
B .
ENDP
ALIGN
;*******************************************************************************
; User Stack and Heap initialization
;*******************************************************************************
IF :DEF:__MICROLIB
EXPORT __initial_sp
EXPORT __heap_base
EXPORT __heap_limit
ELSE
IMPORT __use_two_region_memory
EXPORT __user_initial_stackheap
__user_initial_stackheap
LDR R0, = Heap_Mem
LDR R1, =(Stack_Mem + Stack_Size)
LDR R2, = (Heap_Mem + Heap_Size)
LDR R3, = Stack_Mem
BX LR
ALIGN
ENDIF
END
You meant:
EXPORT __initial_sp
EXPORT __heap_base
EXPORT __heap_limit
Those ?
From there, how do I know, whether it is located at 0x20000000 or at 0x24000000 ?
Thanks,
Manu
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-23 2:37 PM
- Read your map file
- Stop in debugger in your main() and look at the registers. Especially at MSP ;)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-23 4:00 PM
Reading the map file...
Execution Region RW_IRAM2 (Exec base: 0x24000000, Load base: 0x08047920, Size: 0x00026358, Max: 0x00080000, ABSOLUTE, COMPRESSED[0x000000b4])
Execution Region RW_DMARxDscrTab (Exec base: 0x30040000, Load base: 0x080479d4, Size: 0x00000060, Max: 0x00000060, ABSOLUTE)
Exec Addr Load Addr Size Type Attr Idx E Section Name Object
0x30040000 0x080479d4 0x00000060 Data RW 833 .RxDecripSection ethernetif.o
Execution Region RW_DMATxDscrTab (Exec base: 0x30040060, Load base: 0x08047a34, Size: 0x00000060, Max: 0x00000140, ABSOLUTE)
Exec Addr Load Addr Size Type Attr Idx E Section Name Object
0x30040060 0x08047a34 0x00000060 Data RW 834 .TxDecripSection ethernetif.o
Execution Region RW_Rx_Buffb (Exec base: 0x30040200, Load base: 0x08047a94, Size: 0x00001800, Max: 0x00001800, ABSOLUTE, COMPRESSED[0x00000034])
Exec Addr Load Addr Size Type Attr Idx E Section Name Object
0x30040200 COMPRESSED 0x00001800 Data RW 832 .RxArraySection ethernetif.o
It does match the given scatter file.
So:
Current Size: 152kb
but:
0x24000000 - 0x2407FFFF AXI SRAM <-- Current IRAM2: (Size: 0x7ffff, 524287, 511kB)
Heap + Stack = 512kB
512k should be quite enough ..
Somehow, FreeRTOs + LWIP + altcp + mbedTLS cribs about out of memory like a stack overflow, very weird.
crash is around tcp_connect() return, which looked quite weird. FreeRTOS hooks show a happy stack though.
Argh!