2025-01-23 10:52 PM - last edited on 2025-01-27 03:22 AM by Andrew Neil
Hello. I have a problem, I wanted to test the power saving mode on a board with a microcontroller stm32h743vit6. For this, I made a minimal project. Where I switch to stop mode and wake up by pressing the button. Consumption in this mode is about 4.5 mA, which is a lot. I tried to switch to standby mode, and the consumption was 1.5 mA. How else can I reduce consumption??? The board is powered by a battery, all other components are removed from it.
2025-01-24 12:39 AM
Hello,
Try to inspire from the low power examples provided in the H7 Cube here.
@kukoldiega wrote:
all other components are removed from it.
Not sure what do you mean by other components are removed but double check if you have something else consuming on the board.