cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H723ZG Board losing communication

PGM.2
Associate II

Hi all,

Nucleo-144 Stm32h723zg board while debugging suddenly loses communication and shows target not found, unable to read register values. This does not happen always but during debugging this issue is coming up,any solution or any problem with the board can someone help me out.

Thank You.

12 REPLIES 12
mƎALLEm
ST Employee

Hello,

It could be an issue with your USB port: connection issue or couldn't deliver enough current to the board.

It could be due to the USB cable, so try to change the cable.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PGM.2
Associate II

Hi, I have tried using other USB port and USB cable but still I am facing the same issue.

Is there something plugged to the board, I mean another shield, daughter board, device? that get power from the USB? or it's only the Nucleo powered by the USB?

Do you have another Nucleo board to do the same test?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PGM.2
Associate II

Yes I am using a wireless mouse but I have 2 boards actually one board works fine but the other one is facing this issue

mƎALLEm
ST Employee

"I am using a wireless mouse" --> is it connected to the Nucleo over USB-OTG?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PGM.2
Associate II

No it is connected to the laptop using a different USB port

mƎALLEm
ST Employee

Did you try to debug a simple example from CubeH7, for example \Projects\NUCLEO-H723ZG\Examples\GPIO and without modification?

Do you have the same issue?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PGM.2
Associate II

Yes but i did not face any issue while debugging the example code

There are two hypothesis:

1- I suspect an issue with your application, may be a power configuration issue

2- watchdog resetting your micro.

Could you please use CubeProgrammer and provide a screenshot of "User Configuration" in Option bytes menu (OB)?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.