cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H573 PB14

gaso111
Associate II

In our project I use STM32H573VIT6 LDO uC.

We have a problem with the PB14 pin. We use 3 pins for LED control (PB10, PB13 and PB14, see photo). The problem with the PB14 is that the LED lights up dimly without code initialization.

If PB14 is initialized as Output, Open Drain, No Pullup-Pulldown, it lights up dimly in the OFF state and normally in the ON state.

With Output Push-Pull initialization it works normally, i.e. in the OFF state the LED does not light up and in the ON state it lights up normally.

 

1. What could be the problem?

2. Should I use PB14 at all and is there a potential risk of later problems?

27 REPLIES 27

As I said, it is the same state whether code is not loaded (not programmed) or code is running.


@STOne-32 wrote:

Dear @gaso111 ,

I concur what described by @AScha.3  the electronic shared should LED On when GPIO is in output 0 level to GND , either OD or Strong Push-Pull to 0 ( which seems working) . If possible to probe PB13 and PB14 and show us the signals in different combinations.

No pulses, on Pin PB14 I measured (with scope) 1,38V and on other side of resistor R213 I measured 1,50V

That means current flowing in PB14, when OD output is not active (FET is not conductive) is:

(1,50-1,38)/470=0,25mA

On PB13 I measured 1,86V and on other side of R210 the same voltage 1,86V. This means no current flows in PB13 pin.

These two GPIOs are special for USB type C _c as shared by @Tesla DeLorean  and @Imen.D  . We need to understand what is happening with PB14 only as it seems a path / strong leakage is created to ground even in input default state . Also sharing full schematics of power pins and boot is helpful. Let us know 

Ciao,

STOne-32

P.S.

I have uploaded part of the schematic. There is VBAT (pin6)  open. I connected it to VDD (3V3) and a 100nF capacitor in parallel, but no changes, LED201 lights up dimly when PB14 is not active (in OD mode).

 


 

>>I don't think, because the same effect is if uC is not flashed (board is only powered).

And I don't think that's how fuses work..

If what you've wired has established a conduction path, it really doesn't matter. A device with blank FLASH will run from ROM. PB14 is potentially set as an output, per AN2606

If the LED is emitting photons, it's because electrons are flowing, conduction is occurring, resistance is limiting the amount. Put more resistance there so it's not permitting 7mA to flow.

 

https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

So the bootloader is started and sets PB14 as uartTX :

ed: as SPI2 output :

AScha3_1-1718304100713.png

 

When you have flashed a valid program and dont start the bootloader, (boot0 = lo ),

but your program, PB14 will work as you want.

If you feel a post has answered your question, please click "Accept as Solution".

You sure? My AN2606 for the STM32H573 shows it uses PB14 for SPI2_MISO, in a context where the STM32 is the SLAVE device. It's perhaps arguable WHEN that occurs, and if it's only after CS is seen to go low, or at reset. On the UART RX are connected to TIM inputs to measure the 0x7F 8E1 pattern before enabling the UART and UART TX output.

https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf

an2606_u573_pb14.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Ok ok, your right, i just mixed it up (from memory...) :)

AScha3_0-1718303928003.png

usart1 is started on PA 9/10 . 

If you feel a post has answered your question, please click "Accept as Solution".

I think the discussion is going in the wrong direction.

Once again:

1. The board is only powered, no code downloaded to the flash, nothing connected, the LED on PB14 lights up dimly. As far as I know, all GPIOs should be initialized as inputs in this state. A current of 0.25mA flows in PB14.

2. uC is programmed. All three GPIOs (PB10, PB13, PB14) are configured the same, output, open drain (OD), no pushup pushdown. The LED on PB14 lights up dimly again although the output MOSFET is not active ("1" at the output). LEDs on PB10, PB13 do not light up. If a "0" is set at the output, every LED lights up normally (as intended).

3. If PB14 is initialized as push-pull, the LED does not light up when there is a "1" at the output. When "0" is at the output, LED lights up normally (as intended)

Can someone repeat the test under the same conditions and confirm that the same thing happens?

Ok, i tried : on H563ZIT (the "closest" to your chip, i have ) -> PB14 as open drain, hi; green LED to VDD.

 

Program flashed, debug at start : LED lights up dimly ...

-> run program , ok, and : LED lights up dimly ...

(on next pin, PB13 , unused, LED dark. )

So...maybe something wrong with the open drain setting here...on PB14. (I never used this pin before.)

Next : set PB14 to PP mode, hi : LED dark, as it should be.

-> also on my H563ZIT same behavior . Seems to be a chip problem. Nothing in errata.

Maybe @STOne-32 could tell something about this symptom on PB14.

 

So as workaround use push-pull mode, working as it should.

Otherwise there should be no problem , when using it to switch the LED in PP mode.

+

I tested PB14 as input only,  LED lights up dimly ;

on hard reset pressed :  LED lights up dimly.... so permanent 12Kohm pulldown on this pin.

If you feel a post has answered your question, please click "Accept as Solution".

1) When FLASH is blank it will be running the code in ROM, it doesn't just crash into an Out-of-RESET state

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you very much @AScha.3 ,


from the beginning I suspected that there was something wrong with PB14 in OD mode.
I don't know whether and how this will be included in the errata sheet.