cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H563ZIT6 LDO or SMPS?

Ricko
Senior III

Hi,

does the STM32H563ZIT6 have an LDO and/or an SMPS? Contrary to other micros, I cannot find any table or details about it other than the block diagram common to the whole family (screenshot below) and it says "LDO and/or SMPS". Where on the datasheet can I find that information?

Also, on table 14 (second screenshot) which one of the two LQFP columns should I consider (LQFP144 SMPS or LQFP144)?

Datasheet: https://www.st.com/resource/en/datasheet/stm32h563ii.pdf 

Thank you

Ricko_0-1735833059659.png

 

Ricko_1-1735833567941.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

On STM32H5 it's either SMPS or LDO contrarily to H7 which has both configurations on the same package.

This is from the datasheet:

Q stands for SMPS package:

SofLit_1-1735833957236.png

In CubeMx:

SofLit_1-1735834421772.png

SMPS in red, others are LDO.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Hello,

On STM32H5 it's either SMPS or LDO contrarily to H7 which has both configurations on the same package.

This is from the datasheet:

Q stands for SMPS package:

SofLit_1-1735833957236.png

In CubeMx:

SofLit_1-1735834421772.png

SMPS in red, others are LDO.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Ricko
Senior III

Thank you @SofLit