Skip to main content
Associate
December 30, 2024
Solved

Missing "Synchrounous slave" option in SAI settings

  • December 30, 2024
  • 3 replies
  • 676 views

I want to synchronize two SAI interfaces together, but I can not select the "Synchrounous slave" option unless I enable master block in the same SAI. I Have Master enabled in the other SAI and "External Synchro out" as well. When I enable Master in the same SAI, I can even select other SAI as the Sync input. It seems like a bug, but maybe I'm missing something. Im using CubeMX 6.12.0 and STM32H563ZIT6. Thanks

This topic has been closed for replies.
Best answer by STTwo-32

Hello @matyasreznicek 

This has been escalated internally (under internal ticket number 199546). I will be back to you as soon as I have a feedback.

PS: Issue solved on the last release of the STM32CubeMX

Best Regards.

STTwo-32

3 replies

STTwo-32
ST Technical Moderator
December 30, 2024

Hello @matyasreznicek @and welcome to the ST Community.

First, i suggest you try using the last version of the STM32CubeMX V6.13.0. If you still have a problem, please add your .ioc file in a comment.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
December 31, 2024

Thank you for response. I updated the CubeMX, but the issue persists. Here is the .ioc file. I want the SAI2A to be synchronous to the SAI1A, but the "Synchrounous slave" option is grayed out.

Thanks, matyas

 

STTwo-32
STTwo-32Best answer
ST Technical Moderator
January 3, 2025

Hello @matyasreznicek 

This has been escalated internally (under internal ticket number 199546). I will be back to you as soon as I have a feedback.

PS: Issue solved on the last release of the STM32CubeMX

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.